The UM1758 (Description of STM32F0 HAL and low-layer drivers) document has one line definitions it does not explain. There is not description.This answer was very helpful thanks. Had I understood this from the documentation I would have not asked the...
I am still not able to understand the difference between "TIM Input Capture measurement". and "TIM Input Capture measurement in interrupt mode". I have not been able to find code examples.The UM1758 document has one line definitions it does not expla...
I am trying to use one of the timers as a counter. So that it can read external clock pulses. What I understand from your explanation is that I have to use the following__HAL_TIM_GetCompare(&htimX, TIM_CHANNEL_Xto check if the pulse at the input pin...