STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! TIMER interrupt priority using Register in STM32G030K6T6

i am Initialize  UART2 and timer1 then my timer interrupt and UART2 interrupt in working fine but when i set priority timer first they do not set why? void main(void){NVIC-Set-Priority(TIM1_BRK_UP_TRG_COM_IRQn, 0);NVIC-Enable-IRQ(TIM1_BRK_UP_TRG_COM_...

UART Receive Interrupt update global variables

Using UART in Receiving Interrupt mode, I want to update various global variables values from console like Putty.  Something like first send the opcode and then value. Please suggest if any sample codes available. I am relatively new to programming w...

Nico3 by Senior
  • 1050 Views
  • 1 replies
  • 0 kudos

SDRAM signals - FMC_NL and FMC_SDNWAIT

Using STM32H743IGKx.Tools: LinuxSTM32CubeIDEVersion: 1.12.1Build: 16088_20230420_1057 (UTC)STMCubeMXVersion: 6.8.1-RC4Build: 20230419-1431 (UTC)When setting up the SDRAM configuration in MX, I end up with a couple of signals that look like they are n...

Resolved! EXTI not work as expected

 i am using NUCLEO-F410RB boardi followed the simple exti tutorial try to print "button pressed" to uart when the corresponding button is pressedlike most of the tutorial setting : interrupt rising edge . no pull up and pull down , one side of button...

Beam Forming sample for MIC ARRAY

I'm in the first steps of my project. Selected STM32F446ZE Nucleo board for developing MIC ARRAY application as 446ZE used in BLUE COIN and made my own same arranged mic array board. Now I found there is no Beam Forming sample for it!ST has a documen...

_behn4m by Associate II
  • 1869 Views
  • 1 replies
  • 0 kudos

Running 2 uCs instead of 1

Hello,I'm building a device which will have a user control panel with knobs ( adc ), buttons, encoder knobs, and LEDs etc which will use up many pins.  The device will perform time sensitive output tasks such as DAC and PWM based on user input.I'm th...

LMorr.3 by Senior II
  • 2123 Views
  • 4 replies
  • 1 kudos