STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! change pins from gpio to uart

Hi everyone!, in my prototype  i need some low and high pulse before sending uart datas.. How can i do this? I have already tried using HAL_GPIO_Write and HAL_DELAY and it is not worked.I need an advice for it.Thanks.

HAL_FLASHEx_Erase HardFault_Handler STM32G030K8

Hello,I have developed an application that saves accelerometer data when a machine starts up. This data is stored in the last page of the controller's memory (page 31).I'm encountering a HardFault exception that occurs intermittently, roughly 1 in 20...

image.png
sde c.1 by Senior II
  • 8978 Views
  • 18 replies
  • 6 kudos

Resolved! UART Receive issue

Hello,I'm struggling with a really strange issue. I'm trying to make UART RX working on a STM32G4 custom board.I've followed the UART Interrupt tutorial. (https://wiki.st.com/stm32mcu/wiki/Getting_started_with_UART)I've tested it with Nucleo-G431RB a...

EtienneLJ by Associate III
  • 15745 Views
  • 31 replies
  • 0 kudos

Resolved! I2C_DR register wont be cleared

I'm using stm32f103c8 and PCA9685 devices. I'm trying to send data to PCA9685 via I2C bus. I send data using I2C_DR register. But when i write a data to I2C_DR register it sticks to it. After the data is send thee I2C_DR register should be cleared bu...

Clyde_Xander_0-1698781436153.png

I2C stopped working after STM32F411CEU6 is reset

Hi, I've been working with my STM32F411CEU6. I connect my STM with BNO055 IMU sensor that use I2C as its communication protocol. Every time I press the reset button, the program should've start from the beginning, but in my case, that doesn't seem to...

WRama.1 by Associate II
  • 2564 Views
  • 4 replies
  • 1 kudos

Resolved! Low Power Run mode (LPR) frequency and power consumption

I have a few questions about how the LPR works.First off, the RM says "Low-power run mode: This mode is achieved when the system clock frequency isreduced below 2 MHz."1. What is meant by system clock here? SYSCLK or core clock (HCLK)? As far as I ca...

AYash.1 by Associate II
  • 4439 Views
  • 3 replies
  • 2 kudos

Resolved! I2C master remain in timeout status.

Hi, I have a problem with I2C communication between two MCU.The MCU that acts as I2C master in its main loop calls the HAL_I2C_Master_Receive function at an interval of approximately 1 second and reads the status of the MCU that acts as I2C slave.Eve...

FMass.1 by Associate III
  • 4267 Views
  • 2 replies
  • 2 kudos