STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How long is __NOP()

Hello,How long does the __NOP() function last?Is it the time of a cycle? Or 1/F = cycle time?My MCU is an STM32F401RE, and I understand that the maximum frequency is 84 Mhz.So 1/84 Mhz = 11.90 ns, is that the time of a cycle?In my case, if I loop 14 ...

AD_716 by Associate III
  • 11235 Views
  • 9 replies
  • 4 kudos

Resolved! AN2606 missing STM32G4A1 series

I'm trying to configure the Bootloader for a STM32G4A1KE processor, but in the AN2606  I cannot find any information regarding this processor (family STM32G41). Although it is listed in the introduction section of AN2606, no further information is gi...

STM32L433 goes to hardfault after certen time lapse

Hello everyone, I am using STM32L433 with external crystal 12MHz. SYSCLK is 72MHz. i am using three usarts (1,2and 3). but after certain time period of execution lapse. STM32L433 goes to hardfault handler and executiion stucks, After debug found that...

rahulgate by Associate II
  • 12145 Views
  • 7 replies
  • 0 kudos

What is SAI "Error between selected"? (CubeMX bug?)

Today I spent some time to fine-tune SAI clock to get standard 22.05kHz sample output rate.However, I do not understand why CubeMX states that "Error between selected" is 0.22%.What is "Error between selected"? Why this error is zero when selected fr...

SAI3.png SAI2.png SAI4.png
TDJ by Lead
  • 5167 Views
  • 10 replies
  • 8 kudos

Design guied lines for signal integrity

Hi Can i get the STM32L4R9ZIT6 Component Data .Pcb Design and Layout guide for signal integrity.I need simulation validation standards for the above component.Regards.Raneel.

Raneel by Associate
  • 1117 Views
  • 1 replies
  • 0 kudos

Leap year setting in RTC

Is there any inbuilt leap year setting in the onboard rtc of STM32L152RC. If not how to manually configure it. Source code also. Thank You

hazin by Associate III
  • 1376 Views
  • 1 replies
  • 1 kudos

Resolved! Changing PWM frequency with potentiometer

Hi everyone, I am trying to generate PWM signal and change it's frequency with a potentiometer. I have connected an LED to the PWM output and it blinks only a few times and then stops. Sadly, I don't have an osciloscope to check the signal.I am using...

MS.23 by Associate II
  • 10472 Views
  • 7 replies
  • 1 kudos

Resolved! STM32 series PWM out logic level at reset and pause state

I am using STM32F103RCTx and STM32CubeIDE for developing a small application.I am tuning a vacuum pump DC motor using PWM signal with TIM1 CHANNEL_1. But I hit a small problem when I start debug the board. The motor is running from the time the IDE s...

NEdom1_0-1698624497618.png
NEdom.1 by Associate III
  • 3605 Views
  • 4 replies
  • 0 kudos