STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! NUCLEO SRC1M1 X-CUBE-TCPP USBPD Charging problems

Hi, I am using a NUCLEO-G474RE with the X-NUCLEO-SRC1M1 board. I have created and configures the project according to https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB-Power_Delivery_Source I am monitoring the board with the ...

janik by Associate II
  • 666 Views
  • 1 replies
  • 2 kudos

Resolved! Bug in STM32F103: enabling FSMC clock pulls up PB7

I have an STM32F103 board call 野火STM32F103ZE_霸道开发板,i found  enable  FSMC clock will pull up PB7  GPIO to 3.26v ,   i try decrease my code ceaselessly to verify this bug, finaly it can reproduce bug easily like this #include "stm32f10x.h" int main (v...

owlm00n by Associate II
  • 1700 Views
  • 15 replies
  • 10 kudos

Resolved! Execution time changes over time, why?

STM32F411RE - NUCLEOI'm working through a course on power optimization on STM32s & I'm genuinely confused about some results I'm getting off the board. I've set up TIM5 to count execution time in us like so, void Timer_Init_For_Timing(void) { RCC->A...

OCTA SPI PINs For STM32U575VIT6Q Controllers

Hi @Issamos Hope You doing well . we are started new design using STM32U575VIT6Q this controller, we have some doubts regarding the SPI line, we searched in the STM32cubemx in that we cannot able to find the octa spi pins, Can you pls share me the St...

HA2375- by Associate II
  • 322 Views
  • 2 replies
  • 1 kudos

Resolved! Strange variable behavior in struct, TCP / lwIP

Heyho,I have a super-stable TCP-audio-streaming server on a H733 here, using custom ETH driver and lwIP, no OS.But I recently found that in a struct which is used for handling / storing the TCP connection, the variable to store the port number "u16Po...

LCE by Principal II
  • 413 Views
  • 2 replies
  • 1 kudos

Resolved! ISR memory update & Timer trigger

Hello All, I am facing a strange situationI have an ISR function1 that is triggered on Falling / Rising Edge of a GPIO pin This function1 according to the state of variable will either start TIMER2 and stop TIMER3 and the way around.TIMER2 & 3 have a...

vbesson by Senior
  • 509 Views
  • 2 replies
  • 2 kudos

Resolved! Using SPI with DMA

Hi All, I'm using an STM32F1 with a 240x240 LCD screen that comunicates with the micro by SPI (with DMA). The screen uses the ST7789 driver (I supose it is not important). I'm working with RGB565 color format.The problem that I have is, for example, ...

BTurc2_0-1688298032648.png
BTurc.2 by Senior
  • 19665 Views
  • 21 replies
  • 5 kudos

ADC2 calibration

Hi,I have a problem with the ADC2 calibration on STM32H743VIT6(V). I use ADC1 and ADC2 in dual mode(Regular simultaneous mode). On some boards the ADC2 calibartion doesn't work. (The ADCAL-Bit in ADC_CR is not cleard after start).On the boards where ...

LKoe by Associate
  • 2114 Views
  • 6 replies
  • 3 kudos