STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Any limits on flash selection for STM32N6

From my understanding all STM32N6 chips need a external flash chip and there's a static stage 0 boot loader.  So if this is true is there any limitation's on the brands of flash or speed/address bit size limitations? With the previous stage 0 bootloa...

Resolved! RM0456 discrepancy in ADC oversampling right shift

In the RM0456 at 33.4.31 Oversampler it say:The division coefficient M consists of a right bit shift up to 10 bits, and is defined using the OVSS[3:0] bits in the ADC_CFGR2 register.But at 33.6.5 ADC configuration register 2 (ADC_CFGR2), it allow up ...

nicolas by Senior II
  • 510 Views
  • 3 replies
  • 1 kudos

ADC "shorting" analog input to GND

We're using the following circuit to measure a battery voltage @ 20 kHz for use in motor control.We are having some issues though, where the ADC suddenly starts measuring 0 V (0 in the data register) and gets locked in this state. In this state, we a...

DC_bus_measurement.png

Resolved! STM32U5 FATFS with FreeRTOS

Hi,I'm attempting to write to an SD Card using a Riverdi STM32U5A9 display board.  Since TouchGFX natively uses FreeRTOS, I'm attempting to keep it within FreeRTOS.  Porting to ThreadX has caused it's own issues which I have in a separate thread.  In...

co2meter_0-1763562827680.png co2meter_1-1763562850347.png co2meter_2-1763563015363.png co2meter_3-1763563045901.png
co2meter by Associate II
  • 848 Views
  • 2 replies
  • 0 kudos

Resolved! STM32G071GBUx Bootloader Setup Problem

Hi, I am trying to configure my STM32G071GBU6 to enable reprogramming  the flash throguh USART1. I check the datasheet of STM32G071x8/xB, reference manual RM0444, and application note AN2026. It says I am supposed to configure the PA9 (USART1_Tx) and...

YuXiao by Associate II
  • 819 Views
  • 4 replies
  • 0 kudos

PWM jitter on a home made card

Hello everyone, Some time ago I asked on this website information about jitter on a PWM : Solved: PWM jitter - STMicroelectronics CommunityThe problem was that when generating a PWM, it wasn't very stable. At the time changing the source clock to the...

EliazLB by Associate III
  • 1879 Views
  • 9 replies
  • 2 kudos

Error in initializing ST-LINK device

Hello everyone i had today while working with the NUCLEO H753ZI board and when i try to upload the code i had faced this error message when i try to connect with the cube programmer i faced this error and my LD6 pin is glowing with low intensity can ...

Screenshot (5).png WhatsApp Image 2025-11-18 at 8.00.21 PM.jpeg

Resolved! ROM Bootloader - only responds with 0xA5

I have two boards, both with the G473.I am using the ROM bootloader on SPI1. On one board, the bootloader works.  On the other, it only responds with 0xA5 during the initialization sequence.The MCU can program and run if I load it through the SWD por...

JBill.10 by Associate III
  • 954 Views
  • 5 replies
  • 0 kudos