STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Enumeration_USB_VBUS

Hello,let say that STM32H753 mCU has connected VBUS (via resistor divider to be sure that voltage on VBUS detection pin (PA9) would never exceed AMR), D-, D+ and GND lines with PC, before mCU core is supplied. At the moment when mCU core is then conn...

D3jan by Associate II
  • 625 Views
  • 4 replies
  • 0 kudos

Resolved! MIPI-DSI: Low Power Command Transmission

Hello! I'm now using a STM32F469 to drive a screen with MIPI-DSI Interface. I need to send the initial codes with low power command transmission, and then drive the screen in video mode. I think LPDT it is supported by this MCU, but I'm not sure how ...

STM32F427ZGT6 inaccurate delay

Hello, when I was using this chip, STM32F427ZGT6, it could print data, but the delay was incorrect. After 5 seconds, it was only a few milliseconds. Due to the inaccurate delay, the timing sequence became disordered

liwei11 by Associate
  • 468 Views
  • 2 replies
  • 1 kudos

SAI: SPDIF output in all MCUs ?

Heyho,do all SAIs in all MCUs offer the SPDIF output feature?CubeMx and online MCU selectors do not show this info, no time to check 20 more datasheets.For the few STM32 I know and worked or played with (G4, F7, H7) the answer is yes.Merci!

LCE by Principal II
  • 1100 Views
  • 8 replies
  • 2 kudos

STM32N6: External Loader Manager, ISSI Flash

Hello,Hello, in our project we are using an STM32N6 MCU and an external flash from ISSI with this MCU. Datasheet of the flash's link in the below.https://www.issi.com/WW/pdf/25LX-WX032-064.pdfDuring debugging, we read the flash using standard command...

Clyasenth_0-1748356963697.png Clyasenth_1-1748356982432.png
Clyasenth by Associate II
  • 1234 Views
  • 2 replies
  • 0 kudos

STM32F407 RAM Interface impedance matching

Hi Team,As we are going to use RAM – IC CY62136EV30 (TSOP-44) in our new project with ST micro STM32F407ZG (LQFP-144).Do we need any impedance matching for 6-layer board?Can you please suggest the same. Crystal frequency we taken 16MHz for the MCU.Th...

Resolved! STM32N6: Expected DMA/SPI Performance

Hi,I am working on an application for the STM32N6 (using zephyr) that streams data from four SPI interfaces (SPI1, SPI2, SPI3 and SPI6) via Ethernet (UDP). I am using full-duplex SPI transfers and GPDMA1.Everything works fine up to SPI clock frequenc...

Jeija by Associate
  • 680 Views
  • 1 replies
  • 0 kudos