STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H723 BOOT0 and RESET control over UART!

Hi All, I managed to be able to bootload the STM32H723 device using the STM32 Flash Loader (STBootLib) but do not like how I have to pull BOOT0 high and also reset the device right before I program the device and then when the boatloading is done res...

ENort.1 by Associate III
  • 3341 Views
  • 3 replies
  • 0 kudos

Resolved! Launching the application from CubeIde vs autonomously

Hello,I wonder if someone has knowledge about any difference in how variables are initialized and handled when launching an application from CubeIde vs starting up the MCU.My case: I use a STM32H7 and the application runs regularly when I launch it f...

SSorr.1 by Associate II
  • 1320 Views
  • 1 replies
  • 1 kudos

Resolved! STM32F103 CAN filter range of ID's

Hello, I have a set of extended CAN ID's I need to pas the bxCAN filter. I looked at some examples where one ID is passed the filter, but could not figure out how to allow a set of ID's. If my understanding is correct the mask is used to determine wh...

Smdeint by Associate III
  • 16152 Views
  • 10 replies
  • 3 kudos

Handling ECCD error during flash read on stm32l4

Posted on October 09, 2016 at 20:03Hello,I'm building an application with ST STM32L4 that stores information on internal flash (ECC flash on L4). The information is valuable, so the flash programming must be robust to unexpected shut downs including...

seutpxle by Associate
  • 17482 Views
  • 7 replies
  • 1 kudos

Resolved! Short question regarding the contact drillings

Good Morning Ladies and Gentlemen, Could you communicate in a short way the size of the contact drill-holes (stm32f411 - CEU) ?The diameter in AWG size would be enough.We also are interested in further documentation-links regarding it. In student wor...

timbo2023 by Associate III
  • 3804 Views
  • 9 replies
  • 1 kudos

STM32L412 Standby+RTC battery current use

Hi all, The STM32L412xx and RM0394 are quite clear about current use of the micro when in standby mode with LSI-RTC.One thing the docs are not so clear about is the effect of having combined VBATT and VDD pins on the low pin-count packages. With thes...

mwp by Senior
  • 2900 Views
  • 5 replies
  • 0 kudos

Running into restricted memory issues with STM32H742VIT6?

Hello,I'm having issues with software behaving inconsistently and freezing when I add certain lines, try to access certain variables, etc.  I suspect maybe it has something to do with the restricted flash regions in the MCU.  Is there any way around ...

options_target.png
briankaz by Associate III
  • 3762 Views
  • 9 replies
  • 0 kudos

STM32412CG UFQFPN48 MCO2 unexpected power consumption

The STM32F412 chips have 2 MCO pins:The MCO2 pin can have 4 different source clocks:I've noticed that when I change the source from a default one (SYSCLK) to PLLI2S (PLLI2S not enabled) or HSE (not connected), the power consumption is reduced ~0,5mW....

dawidn_1-1703147341553.png dawidn_2-1703148081560.png dawidn_3-1703148251704.png
dawidn by Associate
  • 2206 Views
  • 3 replies
  • 1 kudos