STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F411 RTC 32768 cal Freq only 490Hz

I wonder if any one can help me.The rtc Cal freq produced by the init code below produces on 490Hz.  The RTC clock is loosing about 55 sec in 20 minutes.Is there a way to increase this freq without replacing the crystal? static void MX_RTC_Init(void)...

erastusC by Associate III
  • 49 Views
  • 6 replies
  • 2 kudos

Regarding FLASH Writing to the STM32F410

I have a question about writing to the STM32F410's FLASH.I'm creating a program to write data received via USART to FLASH, but it's not working correctly.The writing to FLASH itself is happening, but the written data differs from what I expect.This d...

shank by Associate III
  • 15 Views
  • 0 replies
  • 0 kudos

STM32F303CBT6 DAC not working with DMA

Dear all,I'm trying to generate a waveform using DAC OUT1.I configured pin PA4 as analog (works)I configured DAC1 without DMA and it worksI configured TIM6 and it works Then I configured DAC with DMA, configured DMA, but output never changes.Where ca...

Resolved! Debug losing connection with Stm32WB55 target

Code is written using stm32CubeMX. Connecting with stmlink V3 Minie. Executing step by step, it appears that debug fails (lose connection) when executing debug_init. In fact debug_init creates the problem when programming pa13.When removing the initi...

GYV by Associate
  • 91 Views
  • 8 replies
  • 1 kudos

Cube-AI Software Pack Utilization Problem

Unsure if this has been answered before, however, upon activating the Cube-AI Core and application software pack, the remains static, ie it stays blacked out with a gear icon next to it referring me back to the software packs screen, which already sh...

jdudley9_0-1770405548437.png jdudley9_1-1770405580305.png