STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1575 Views
  • 0 replies
  • 2 kudos

Resolved! SNMPV3 with NUCLEO-H743ZI2 board

I tried enabling the LWIP_SNMP_V3_MBEDTLS and LWIP_SNMP_V3_CRYPTOCan in CubeMX and generated the code, then it is giving me an error as some header files are missing and which are related to MD5 and SHA.  In CubeMX, They have mentioned “LWIP_SNMP_V3 ...

sushma by Associate III
  • 6228 Views
  • 8 replies
  • 1 kudos

cubeMX 6.12.0 and below generates wrong I2C timings

HiI have problems with the I2C frequency when I'm generating code with CubeMX 6.12.0 for the STM32U5A9. The timing register from the I2C3 is generated wrong, which leads to a frequency around 350kHz instead of selected 400kHz in FastMode operation.Th...

nobody_1-1723798827523.png nobody_2-1723798855597.png nobody_0-1723797837248.png
nobody by Associate II
  • 1635 Views
  • 2 replies
  • 0 kudos

start code execution problem with MX_LWIP_Init

HiI add ethernet communication to my program with STM32CubeMx and I just compiled and run it. I have a problem:if I disconnect Jlink the board I have a ping error. but I run the code with 3 times click on run in MDK-ARM the board will ping.I also try...

S_bgh99 by Associate III
  • 5842 Views
  • 8 replies
  • 1 kudos

STM32H7 CubeMX HAL does not switch internal ADC channels

I just updated to CubeMX 6.12.0 and Firmware Pack STM32Cube FW_H7 V1.11.2.  I noticed that the internal ADC selection (for ADC3 on STM32H750) is only partially working.  The first time you select an internal channel, it works.  However, if you then s...

DPade.1 by Associate III
  • 2244 Views
  • 3 replies
  • 0 kudos

Resolved! USB CDC ACM AND AUDIO DEVICE

I can not find any complete project for USBX or TinyUsb library to drive. Can anyone to help me please?i need USB CDC VCP AND AUDIO DEVICE simultaneously in custom board.   

nimaltd by Senior
  • 2485 Views
  • 3 replies
  • 2 kudos

Resolved! STM32CubeIDE does not recognize STM32CubeMX update

I am using:STM32CubeIDE  Version 1.11.0STM32CubeMX  Version 6.7.0I used STM32CubeMX to update itself to Version 6.12.0  (to location C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX)Problem:I cannot open/edit BLE_HeartRate.ioc file because i...

JimEno by Associate III
  • 2130 Views
  • 2 replies
  • 0 kudos