STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1570 Views
  • 0 replies
  • 2 kudos

Resolved! Help installing STM32CubeMX IDE

Hello, I want to get started using ST microcontrollers. My work computer does not have an internet connection so I need some help installing the software on this computer. I want to use the STM32CubeMXI have downloaded the installation file onto a di...

JLIND.1 by Associate III
  • 3392 Views
  • 4 replies
  • 3 kudos

Resolved! BUG: Cube MX cant create project for STM32U031K8U6

Hi,I'd like to create a project using your STM32U031K8U6 device, but it seems, that the project template is corrupt.Creating a project by access MCU selector->STM32U031K8U6, start projectProblem is reproducible on 2 computers. Tried already Help->ref...

froesel_0-1723196207648.png
froesel by Associate III
  • 1956 Views
  • 3 replies
  • 0 kudos

stm32cubemx and keil

if you want to use ADC to DAC and have 200hz output. what is the first thing to do? connect the ADC to the DAC or set the output frequency first until it reaches 200hz?

Resolved! STM32CubeMx Ubuntu 22.04 [ERROR]

Bom dia!Instalei o STM32CubeIDE no Ubuntu 22.04, e não consigo criar um novo projeto.Ao Iniciar o CubeMX, consigo selecionar o MCU desejado e, na sequencia, retorna a seguinte mensagem de erro:Executando o IDE via terminal, no momento do erro apresen...

LeoContini_0-1723211381344.png

Resolved! SINE WAVE DAC IN STM32CUBEMX

I have a DAC signal from an ADC (potentiometer). I have set the frequency from 0-200 Hz but when I run it when I am at 200 and the sign should still be there, the signal on the oscilloscope disappears (just a straight line). does anyone know how to f...