cancel
Showing results for 
Search instead for 
Did you mean: 

Can MSI be changed on the fly when used as system clock source?

chien
Associate

Hi,

I am using B-L475E-IOT01A. I am wondering that MSI can be changed on the fly when it used as system clock source.

In `HAL_RCC_OscConfig` from STM32L4Cube drivers code, it looks like ok. But I didn't find any relative information from l47xxx manual. The manual only specifies that MSIRGSEL can be modified when MSION is 0 or when MSIRDY is 1. Not allow changing it when MSION is 1 and MSIRDY is 0.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
TDK
Super User

Yes, it can be changed on the fly.

Restrictions would be listed in the reference manual.

If you feel a post has answered your question, please click "Accept as Solution".