STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F USB High speed real throughput

Hi,we have developed a board with a low resolution camera interface using an STM32L0xx MCU.Now we want to use an HD camera and for this we have a module supporting USB2.0@30fps of 1920H x 1080V frames on USB, so it is really important to use a USB HS...

STOMPOU by Associate II
  • 6161 Views
  • 8 replies
  • 0 kudos

Resolved! How to do USB DFU from a custom MS visual studio application?

Hi all,I'm investigating what I need to be able to update the firmware on my custom STM32 board (with either an STM32H7 or STM32F7 MCU) from a C#/C++ Microsoft Visual studio application via USB. This is for Windows 7/10/11.I found STSW-STM32080 but i...

Rodo by Senior
  • 2610 Views
  • 2 replies
  • 3 kudos

Resolved! STM32H750 RAM configuration

I am looking into RAM support for the SMT32H750 series chips for my future projects.The STM32H750 series chips support 16-bit data bus as well as 32-bit data bus configuration. This mode is selected on startup, as far as I can tell.If I were to use t...

etamarin by Associate III
  • 3534 Views
  • 7 replies
  • 5 kudos

Resolved! ADC sampling rate checked by callback

Hello,I am using a NUCLEO-H743ZI2.I read the reference manual RM0433 Rev8.I also read a bunch of topics in the forum but didn't find what I wanted. I am trying to check my ADC sampling rate by looking at the timestamp at my half full/full callback fr...

ADCclock.png formulaFadc.png ADCconfig.png ADCdoc.png
Kévin by Associate III
  • 4742 Views
  • 5 replies
  • 2 kudos

Resolved! STM32G0 - G0B1RE GPIO MOD REGISTER not enabled

Hi, I use STM32Cube IDE, and use STM32G0 - G0B1RE device. I try to enable the mod register to blink the LED here is the code that i try so far, based on the Reference Manual (rm0444), I need to enable RCC_IOPENR before modify the GPIOx_MODER. But unf...

Screenshot 2024-01-19 at 09.21.06.png Screenshot 2024-01-19 at 09.23.59.png Screenshot 2024-01-19 at 09.24.22.png Screenshot 2024-01-19 at 09.24.32.png
dx7 by Associate II
  • 2352 Views
  • 4 replies
  • 0 kudos

Resolved! profibus

Hi community,any mcu from family STM32H7 or other that supports Profibus?Thanks a lot

SGasp.1 by Senior
  • 2263 Views
  • 1 replies
  • 1 kudos

STM32F103C8T6 flash memory size

Hi, I tried to read BluePill board MCU STM32F103C8T6 flash by STM32CUBE in Target information it shows Device ID 0x410 and flash memory size 128kb but by datasheet STM32F103C8T6 flash memory must be 64 kb Why is the difference?  

Einar by Associate II
  • 4681 Views
  • 5 replies
  • 6 kudos

Erased Option Bytes resulted into bricking STM32U5A9J-DK

Device: STM32U5A9-DKBootloader AN: AN2606Reference Manual: RM0456I was trying to enter the system bootloader (UART mode) through programming the NBOOT0 and NSWBOOT0 bit which is present in the FLASH_OPTR register of the option byte region.Now, this w...

Screenshot (195).png Screenshot (192).png
Deblina by Associate II
  • 2142 Views
  • 2 replies
  • 0 kudos

ART-PI dev board STM32H750 FMC+LTDC+RGB888 display

Hi all!I wrote code on my ART-PI development panel that displays a simple filled box and text (touchgfx). I use the following in both projects:FMC with 240Mhz, SDRAM with 120Mhz. W9825G6 data 16bitCPU clock 480MhzRGB888 display, MRG7122 DCLK typical ...