STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G431 - ADC + DMA using HAL not working

Hi,I am trying to make the ADC + DMA work a STM32G431CBT6 using STM32CubeIDE and the HAL library. I am used to making it work on other families like the STM32f103 etc.. However, here, when I program the processor using the debug mode and watch the co...

Resolved! How to use HAL_UART_Receive_IT to receive uart data?

Hi all, What is the correct flow to use HAL_UART_Receive_IT() to receive uart data?The first package is lost first its first char,Here is the flow used now, From the gif, you can see "H" is missing for 1st package, and all normal for others.The probl...

HAL_UART_Receive_IT.gif
E-John by Associate III
  • 15767 Views
  • 6 replies
  • 4 kudos

Feedback Requested on general approached used for ADC

Hello, reaching out to see if anyone can provide some thoughts on a project I'm working on.  The project works but though I'm a longtime Arduino developer this is my first STM32 project - so not 100% sure of some of the parameters I've chosen are the...

Joystick.png adc.png
nollstead by Associate III
  • 1313 Views
  • 0 replies
  • 0 kudos

Overflow interrupt problem stm32f1

Hello, I have a problem currently, I am a beginner on stm32 and I would like to create a pulse counter but I cannot get the interrupts from my timer 3 to increment my variable. I don't understand then that the function is indeed carried out but it is...

Resolved! STM32U575I-EV DCMI example, expected performance

I am currently using the STM32U575I-EV; I was able to flash the DCMI example project's code from STM32CubeU5 (Projects\STM32U575I-EV\Examples\DCMI\DCMI_ContinousCap_EmbeddedSynchMode) and I see the onboard camera's feed displaying on the LCD as expec...

Resolved! std::remove_if broken?

Hi everyone,I have an odd behaviour here. I got a STM32L496 with FreeRTOS on it. The CPU is very busy (15 task running, flash size is almost 1MB). I am using the latest STM32CubeIDE 1.14.1.Now I'd like to remove something from a std::vector, so I do ...

JE by Associate III
  • 8484 Views
  • 3 replies
  • 0 kudos

Using ARM CMSIS/DSP libraries on STM32U5

Hi,I want to migrate a project that I have made on a STM32L4 where I make the spectral analysis of the noise that I read from a digital MEMS microphone using the arm_fft dsp functions to a new board with a STM32U5 mcu.I have tried to include the "lib...