2023-10-26 11:06 AM - last edited on 2024-09-24 05:21 AM by Amel NASRI
Hi!
I am using an STM32F103C8T6 mikrocontroller and i program with makefile and VsCode. I use the CAN on it and i need to work with STDID and a EXTID. On the bus there is dozens of standart CAN messages and sometime exteneded messages. From the standart ID-s i just need which identifier is 0x7C1 and next to that i need the all exteneded messages too. I would like to direct the standart messages in FiFo1 and the extened to FiFo0 (or inversely doesnt matter just one FiFO for the extened and other for the standart). I have created two canfilterconfig like this:
For the exntened:
Solved! Go to Solution.
2023-10-27 08:01 AM
i think i figured out what was the problem. I have made a new project where i just use the CAN and the filter configulation. I configured the FiFo 0 to catch just 0x7C1 is filter list mode just like that:
2023-10-27 08:01 AM
i think i figured out what was the problem. I have made a new project where i just use the CAN and the filter configulation. I configured the FiFo 0 to catch just 0x7C1 is filter list mode just like that: