STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G474 release fifo

Hi all,I used long time STM32F103 and there was the possibilty to release the CAN Fifo by writing CAN_RF0R, resp. CAN_RF1R register. For G474 I didn't find this possibilty. Has someone any idea how to release the receive buffer or is the only option ...

CDril by Associate
  • 647 Views
  • 0 replies
  • 0 kudos

stm32u585 UART receive not working, transmit working

HiI have been using stm32u585QII3 MCU in our custom board. I am using USART1(PB6, PG10) to transmit and receive data. In interrupt mode transmit call back is working but receive call back was not working. Initially i have set a break point, the inter...

IP UART TRANSMIT.png IP UART RECEIVE.png
_Danny_ by Associate III
  • 2797 Views
  • 5 replies
  • 2 kudos

Validating received UART message

Sorry if this is a rookie question. I have set up USART 2 to receive a UART command. If the sent command is "<EN>", I need to toggle the value of a global state variable. When transmitting the received data via the callback interrupt, I have no issue...

HAL_UART_Receive_IT not resetting after HAL_UART_Transmit

I am trying to implement MODBUS protocol. STM32 receives an initial message of 8 bytes and then send a response of 8 bytes. However, the next message received by the STM32 doesn't trigger the HAL_UART_Receive_IT callback. uint8_t reception_complete =...

jlaufer_0-1710358749228.png
jlaufer by Associate III
  • 2071 Views
  • 3 replies
  • 0 kudos

STM32U5A5 USB device vendor specific class implementation

Hi,I need to create a USB composite device class interface with STM32U5A5 controller. I have been using the USB_CDC_ACM example project so far for my development. In this example the USB CDC ACM class is configured and I need to change/add this to a ...

Kannan1 by Associate III
  • 2186 Views
  • 1 replies
  • 1 kudos

Resolved! STM32H755ZIT

Hello, Does the STM32H755ZIT support flashing over CAN? The application note AN2606 suggests that the H75x series does support bootloader access on the FDCAN1 interface, but specifies pins PH13 and PH14, which are not available on the LQFP144 package...

ahuster by Associate
  • 2255 Views
  • 4 replies
  • 5 kudos

Resolved! FLASH_VOLTAGE_RANGE_1

Hi,What is the effect of "VoltageRange " while erasing a sector ?  Er.VoltageRange = FLASH_VOLTAGE_RANGE_1; Ret = HAL_FLASHEx_Erase(&Er, &SectorError); #define FLASH_VOLTAGE_RANGE_1 0x00000000U /*!< Flash program/erase by 8 bits */ #define FLASH_VO...

andy_long by Associate III
  • 1909 Views
  • 1 replies
  • 1 kudos