STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Where is ETH_PHY_INTN

In the reference Manual of STMH730, on Table 543, page 2825, there's a Port "ETH_PHY_INTN" listed. Where ist that port? Or where can I configure the GPIO to use for it? I cannot find anything in the datasheet.

SPI MX config buggy?

Hi, i try migrate some old stdlib app into HAL or LL over new project in MX. On old system we have SPI init part for TX only master /* SPI configuration -------------------------------------------------------*/ SPI_I2S_DeInit(SPIx); SPI_InitStruc...

MM1_0-1713285234593.png
MM..1 by Chief III
  • 1416 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F405 TIM1's repetition counter

I have a question when I read the reference manual of STM32F405, and it says that "for odd values of RCR, if  the RCR was written before starting the counter, the UEV occurs on the overflow (which should be underflow  as I have seen in TIMx_RCR funct...

Jerry_ by Associate
  • 5424 Views
  • 4 replies
  • 1 kudos

external loader what is the difference .stldr and .FLM ?

I see that Keil is using .FLMand .stldr looks like CubeIDE are those the same ?can I change the extension from .stldr to .FLM and load using Keil and vice versa ?also any idea how to add the loader to keil ?I see that Keil has a lot pre defined loade...

MNapi by Senior III
  • 2904 Views
  • 4 replies
  • 0 kudos

Where to find ETM version for any specific MCU

Hello, I would like to pick an MCU based on ETM version available on it. This is needed to try out Orbtrace Mini tracing device. It is stated that its currently support ETMv3.5, also i am willing to test lower ETM version and higher too to check the ...

retif by Associate
  • 2090 Views
  • 3 replies
  • 1 kudos

Resolved! Core Locked Up

We have a custom PCB with a STM32H750 on it with Dual NOR Flash (W25Q12BJVSIM). I have been able to flash the code on all but one board. When I attempt to flash the board with STM32CubeProgrammer, I get a Warning: The core is locked up message. How d...

MAlan.1 by Associate III
  • 4258 Views
  • 6 replies
  • 3 kudos

STM32L4S5 Apparent discrepancy in maximum PLL clock

Hi There,I'm trying to set the clock configuration of an STM32L4S5 and have spotted some ambiguities in the reference manual concerning the maximum input frequency to the PLL:RM0432 6.4.4 says the following in the context of choosing the M value when...

BUSY bit in I2C->SR2 gets stuck high when initializing SDRAM

I'm using an STM32F429ZIT6 chip.In my program, the BUSY bit within I2C->CR2 becomes set and never returns to clear. I have verified on a scope that both the SDA and SCL lines remain high during this time and yet the bit remains set. The SR1 register ...

TDK by Super User
  • 3330 Views
  • 4 replies
  • 0 kudos