cancel
Showing results for 
Search instead for 
Did you mean: 

SMT32F407VGT6 / CAN issue

JACK00
Associate II

The CAN communication between the main control board (SMT32F407VGT6) and the same server board (STM32F407VGT6) shows that the ambient temperature is below -10 degrees, the communication is abnormal, and the ambient temperature is above -10 degrees! Immediately returning to normal, may I ask what the reason is? Confirm that the CAN communication interface hardware chip meets the requirements!

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Check performance of external clock and transceiver. 

You can output HSE via PA8 (MCO) and check clock accuracy within specification limits. 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..