STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Enable UART TX over ST-LINK/V2 on unused SWO pin

Hello, maybe a lame question, but how to force enable SWV even if the microcontroller in the project does not support it? Or use ST-link's SWO as console input? (does not have to be SWV)I got a project in Cube IDE for STM32G071KBU3 microcontroller us...

Jkman_0-1714989967264.png
Jkman by Associate
  • 943 Views
  • 0 replies
  • 0 kudos

STM32U575 SPI data size issue

Hi,I am using STM32U575VIT6Q in a BPSK receiver. The STM32U575 SPI1 is set to slave, receiver only. GPDMA channel 6 is linked to the SPI1 input and buffering input data to a data array. The SPI1 clock input (PA5) is connected to TIM1 channel 3 output...

hguan by Associate III
  • 3894 Views
  • 5 replies
  • 0 kudos

Resolved! USART3 offset bytes when receive for the first time after boot

Hello, I am using a nucleoH743ZI2 and STM32CubeIDE v1.13.2 on windows10I configured the USART 3 in order to receive some telecommands from my laptop (windows 10) using a software (HTerm v0.8.9)The telecommands are written in binary, 52 bytes, but the...

USART3conf.png USART3confDMA.png
Kévin by Associate III
  • 2267 Views
  • 3 replies
  • 3 kudos

Resolved! STM32H743 ADC can capture the maximum frequency of sine waves

The maximum sampling rate of STM32H743 ADC1 and ADC2 is 3.6MSPS. According to the aroma sampling principle, the maximum sine wave frequency that can be collected is 1.8MHz. I don't know if I understand it this way, right? I want to collect higher-fre...

hanqingze by Associate III
  • 2564 Views
  • 3 replies
  • 2 kudos

STM32F722 clock initialization error

Hi,I'm working on a project that uses STM32F722RE and I wanted to set the system clock to max value of 216 MHz using 12MHz external crystal as the input for the PLL. The problem is, if I set the SYSCLK and HCLK to 216 MHz, the code fails to initializ...

Roach by Associate II
  • 5753 Views
  • 11 replies
  • 0 kudos

Resolved! STM32G0C1RET6(ARM® Cortex®-M0+ STM32G0 Microcontroller IC 32-Bit Single-Core 64MHz 512KB (512K x 8))

Hi,          (STM32G0C1RET6  for this part number ARM® Cortex®-M0+ STM32G0 Microcontroller IC 32-Bit Single-Core 64MHz 512KB (512K x 8) FLASH 64-LQFP (10x10))two type of pin descriptions have mentioned in the datasheet, I confused which one I have to...

lqfp.png
murali by Associate III
  • 1207 Views
  • 1 replies
  • 0 kudos

Resolved! Ethernet configuration issue

HI STM team,I am using NUCLEO-F439ZI BOARD. I am new to this board. According to the basic configuration the ETH selection shows the warning symbol, reference based on the internet example, the ethernet configuration it does not show the PHY Address ...

Ramachandran1992_0-1714455846651.jpeg Ramachandran1992_1-1714456093524.png

Pin function Spreadsheet

Does ST provide an excel or CSV form of a pin functionality spreadsheet, to aid in assigning pin connections during development? This would be similar to Table 13 in the datasheet, but not in PDF form.

Stan0402 by Associate II
  • 11514 Views
  • 11 replies
  • 3 kudos