STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F051 Internal comparator configuration

Hi,I am trying to configure the internal cooperators in the STM32F051 micro-controller, but in the .ioc file I am able to configure only one Comparator. I require three comparators for my application. Is it possible to configure multiple comparators ...

Aiswarya1 by Associate II
  • 1233 Views
  • 7 replies
  • 4 kudos

I2S clock soruce - internal MSI RC or external HSE ?

I am using I2S (SAI) on the STM32L433 nucleo board and using the internal MSI RC as the clock source.I also have a 32.768kHz LSE external crystral which I believe helps to make the MSI RC clock more accurate when used with PLL.Is the internal MSI RC ...

freeflyer_0-1766003498399.png freeflyer_2-1766003858857.png

Choosing Internal vs external Clock

I do a project with the newer STM32 G , C series and i am curious what are the benefits of external clock vs using the internal clock, because it will save cost and layout space ?

DJMicro by Associate
  • 856 Views
  • 2 replies
  • 0 kudos

BiSS-C Encoder feedback on EVSPIN32G4

Hello, as in this post i'm linkingIs there a way to use absolute encoders/resolvers ... - STMicroelectronics Communityi need to use a Biss-c absoulte encoder for a servo drive application using BLDC motors with STSPIN32G4, we are testing using EVSPIN...

Resolved! Changing the pin connections on the STM32F407VET6

Hi.I have Uart pins (Rx/Tx) PA3 and PA2 on STM32F407VET6. Can these pins be changed to I2C (SDA SCL) in the program?Are the pins on STM32 that have been assigned a protocol (SPI/I2C/Uart) constant and cannot be changed or replaced?Thank you.

No_Name by Associate III
  • 963 Views
  • 7 replies
  • 1 kudos

STM32F407 Option Byte 0xFF, bricked chip

Hi fellows,I have a custom board with STM32F407VGT6. The board was able to be programmed via the JTAG (4 wire JTAG interface; Boot pin is pulled low to ground and reset is connected to the JTAG interface (Nrset pin)) with a segger programmer - multip...

Ratschaka by Associate II
  • 1141 Views
  • 12 replies
  • 1 kudos