STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! stm32h747i-DISCO display issues

I recently bought an stm32h747i-DISCO and tried to run 2 example projects the "JPEG_DecodingFromFLASH_DMA" and the "JPEG_MJPEG_VideoDecoding". Both of them run correctly on M7 processor, but it seems the display has an hardware problem because it tur...

AFato.3 by Associate II
  • 3652 Views
  • 3 replies
  • 1 kudos

Resolved! Is it ok to connect VDDIO2 Pin to VDD?

Hi,I am using STM32L071C8T6 which has a VDDIO2 power pin. I don't see any information on this pin in the STM32L0xx hardware dev reference. My application doesn't require a separate level or source for any GPIO's, so can I connect VDDIO2 directly to V...

icecats_0-1716374212586.png
icecats by Associate II
  • 1314 Views
  • 1 replies
  • 0 kudos

How to make a external NAND flash program algorithm?

Hi all,I am trying to program some data to an external NAND flash chip(connected by FMC) by STM32F429BI with MDK IDE.According to the ARM document, I make a project(download it in the attachment) to generate the FLM file.(Before compiler the project,...

Junde_0-1716370895046.png
Junde by Senior III
  • 1668 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F303VET - issue in transmitting CAN messages

I am having an issue in transmitting CAN messages, my situation is the following:There is an interrupt function for RX messages from CAN1, when a message is received, it sets a flag. The baud rate of the RX message is 10ms and they are being sent ove...

GComes by Associate III
  • 3893 Views
  • 7 replies
  • 1 kudos

Not getting proper response from CR95HF

I am trying to read NFC tags using the NFC03A1 NFC Module and the NUCLEO F439ZI, but I am not able to establish the connection.After sending the ECHO Command (0x00 0x55) and then sending the POLL control byte (0x03), when I read the response using HA...

STOP Mode - USB HID Wakeup

hi all and  @waclawek.jan @Lubos KOUDELKA USB - HID -Keyboard is working fine and keycode coming properly . Enter to STOP mode is successful by HAL_SuspendTick(); HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);Trying to wakeup fro...

MMARI1_0-1716195704237.png
MMARI.1 by Senior II
  • 3669 Views
  • 7 replies
  • 0 kudos

Problems with Comparator/DAC on STM32G473

Hi,I've been struggling with using the STM32G473's internal comparator and DAC for a few days now.ComparatorI use the internal COMP1. For the negative Input I selected the DAC3-CH1 and for the positive input I selected the Pin PA1. PA1 is configured ...

Moritz1 by Associate III
  • 3556 Views
  • 2 replies
  • 0 kudos

STM32G473 BFB2 Not Working

BFB2 Set, but never enter Bank2 program.Boot0 = 0Boot1 = 1I can run the 2 programs from cubeide in there respective locations and ISR work when BFB2 is set for the BANK I am debugging in. However I never enter BANK2 program on resetting/powercycling ...

kip18 by Associate III
  • 5250 Views
  • 5 replies
  • 0 kudos

Jum to Bootloader from application without PIN.

Hi,I am developing a bootloader, I would like to flash the STM32 using another MCU using USART.My question is, If it possible to enter into bootloader mode without using external pins? I would like to enter just by software, is that possible?I see th...

mtapia by Associate
  • 1916 Views
  • 3 replies
  • 0 kudos