STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CAN transceiver-less communication for only two nodes

Question moved from this post. If I have two devices on the same PCB. say an F7 and an MP157, can the CAN_TX of one be connected to the CAN_RX or the other without a CAN transceiver? Similar to UARTs on the same PCB. Maybe series resistors would be r...

inky by Associate II
  • 1085 Views
  • 9 replies
  • 5 kudos

Resolved! About the pins and pin descriptions of the STM32H7S3A8I6

 Hello, I have a question about STM32H7S3A8I6 MCU.https://www.st.com/resource/en/application_note/an5935-getting-started-with-stm32h7rx7sx-mcus-hardware-development-stmicroelectronics.pdfLooking at Table 2 of the description in the PDF above, for gra...

Woongi_0-1768522242502.png
Woongi by Associate
  • 432 Views
  • 3 replies
  • 2 kudos

Resolved! Which stm MCU for LOW speed USB 1.1 device?

Hello, What can i take for a MCU which has function with Low Speed USB 1.1 ? I must make a USB HID Interface as Gamecontroller. It is essential to prevent the PC from getting stuck on the USB port, and this is only possible with USB 1.1.   greets Ste...

stefangem by Associate II
  • 849 Views
  • 12 replies
  • 0 kudos

100% compatible STM32C031G6U6 drop-in replacement

Hi,is there a 64Kb drop-in replacement for the STM32C031G6U6 (which is only 32kb)?We need to find a part where - ideally - we just use the same code without any mods, this is the most important part.And is there perhaps a tool that helps with that? O...

Ricko by Senior III
  • 423 Views
  • 3 replies
  • 0 kudos

Resolved! STM32C071 NUCLEO Start USB DFU Bootloader

Hi,how do I start the USB DFU Bootloader with a STM32C071 Nucleo? I tried it while putting Boot0 to high and pressing reset or do a power cycle but the STM32 DFU does not show up in the device manager. I connected USB to the NUCLEO extra USB port of ...

Resolved! Can not jump to APP from bootloader on STM32G0B0CET6

Hi I have a question that blocked me for several days, Hopefully someone can help, thanks a lot.1:MCU:STM32G0B0CET6,Develop tool:STM32CubeIDE2:I wanna have a test for OTA ,so i create a bootloader project and app project3:Flash segmentation:1)Bootloa...

sg0993_0-1767521397710.png sg0993_1-1767521424042.png
sg0993 by Associate II
  • 1095 Views
  • 10 replies
  • 7 kudos