STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Expanding SRAM on STM32H723VGH6

Hi everyone,I'm a beginner, and this might be a basic question for many of you, but I appreciate your help nonetheless.I'm working on a project using the STM32H723VGH6 (due to size and design constraints, I can't use the ZG series) and I want to expa...

屏幕截图 2024-05-27 015513.png Screenshot 2024-05-28 011839.png sirin_0-1716830413695.png
sirin by Associate II
  • 4532 Views
  • 6 replies
  • 4 kudos

stm32 GPIO Configuaration

I am using a pin to Switch on the power supply once the MCU is powered.When powering up the MCU I am getting a Glitch before it turns on the MC GPIO configuaration is given below. For every output I am getting a glich before it SET from RESET   Can a...

meena by Associate III
  • 1754 Views
  • 3 replies
  • 2 kudos

Using BC1.2 in STM32G473CE

Hi,I want to use BC1.2 protocol of STM32G473CE MCU. But STM32G473CE supports USB PD also. So in order to use only BC1.2 can I use only Dp Dm lines of STM32G473CE and leave CC lines un-connectedAlso what is the maximum power negotiation performed by S...

PY.1 by Associate II
  • 1340 Views
  • 1 replies
  • 0 kudos

UART in STM32-L432KC

This is regarding the UART1 and UART2. 1. I am trying to learn how UART works by communicating between STM32 and ESP32. I am able to send data from STM32 to ESP32 and it works. However, when I do the same from ESP32 to STM32, for some reason I cannot...

Abijith by Associate II
  • 5844 Views
  • 9 replies
  • 1 kudos

SMBus blocked and how to recover it

Hi ST tesam,When I use the HAL of STM32C031, I have some trouble about SMBus.Q1:When I use the SMBus of STM32C031 series. If I do not got the feedback from the slave, sometimes the SDA will pull down(similar to the yellow line show as below) and syst...

LsnLeeJW_0-1719216894031.png
LsnLeeJW by Associate II
  • 1126 Views
  • 0 replies
  • 0 kudos

Resolved! How to configure STM32F407VG using Ethernet in ENC28J60

Hi Team, where we are trying interface ENC28J60 in STM32F407VG Microcontroller to use Ethernet, Is there any procedure to create a project in cube ide are any link related to this board how to interface ENC28J60 to STM controller. Best Regards,Gagan ...

ggowd.1 by Associate III
  • 5242 Views
  • 7 replies
  • 2 kudos