cancel
Showing results for 
Search instead for 
Did you mean: 

GPIO Problem

changhyunkim
Associate

 

Hello, I am having an issue with the STM32 GPIO. The problem is that immediately after supplying power to the chip, GPIOs such as PJ0, PJ1, PJ2, etc. are momentarily powered, behaving as if they were set as outputs.

Below is the test sequence:

1. I created the project without setting the GPIOs and then performed program verification on the chip.
2. I turned the chip off and then back on.
3. I monitored the power supply line of the chip and specific GPIO using an oscilloscope.
4. The result showed that when the power supply voltage increased to above 1.7V, the GPIO voltage also increased.


I hope this helps!

changhyunkim_0-1710748589375.png

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

Are the pins connected to anything? If not, don't assign any significance to pins that are floating. They can be influenced by any number of things, including cross-talk on the board.

If you need pins to have a defined state at reset, use an external pullup or pulldown.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
TDK
Super User

Are the pins connected to anything? If not, don't assign any significance to pins that are floating. They can be influenced by any number of things, including cross-talk on the board.

If you need pins to have a defined state at reset, use an external pullup or pulldown.

If you feel a post has answered your question, please click "Accept as Solution".

Thank you, TDK

We are used a output pin. But, nothing a external pullup or pulldown.