STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

w25q128 external flash with stm32l412

Hi,I am using stm32l412 controller with an external flash w25q128 in quadspi mode. I am able to read and write on to the flash memory. but I am unable to use it as an external loader. I referred many tutorials, I edited the linker script to add a sec...

hash002 by Associate II
  • 1989 Views
  • 3 replies
  • 0 kudos

Resolved! STM32 MCU die

Hi all,Can anyone confirm if these two type of STM32 MCU, STM32H753BIT6 and STM32H753VIH6 use the same die although they have different packages? Best fourhes

fourhes by Associate II
  • 2613 Views
  • 4 replies
  • 5 kudos

Resolved! Alternative Functions and Additional Functions

STM32L072 has USB as Additional Functions instead of an Alternative FunctionThough in one of my Earlier Post It was briefly explained, It felt to have a Dedicated Post in General Thereby this Post to Better Understand the Difference and Way of Workin...

Pavan_LohiaGroup_0-1724038285746.png

Resolved! STM32F411CEUx USB Serial Port Issue

I am having trouble configure the USB-C port for serial output. The board I got is a "BlackPill" and I have went to try some example code for USART2 and USART6, however, upon a reset, I still do not have a COM port appear. Any advice?

dlaroche by Associate II
  • 1410 Views
  • 1 replies
  • 1 kudos

The MCU requires NRST to be toggled after power on

Hi all, I have a problem with a new version of an existing PCB using the STM32F334C8T6 microcontroller.Known working code is loaded onto the new PCB, power is applied and the MCU starts up the clock and then seems to sit idle. If the NRST pin is then...

PXL_20230922_103355658.jpg PXL_20230927_100625674.jpg
RobertK by Associate III
  • 19353 Views
  • 38 replies
  • 8 kudos

STM board not recognized

Hi, I'm currently using Nucleo-U575ZI-Q.I've done nothing to it except leaving it for a day and just plugged it to my laptop again but it doesn't recognize my board now.When I connect it with my laptop, fail.txt shows up with a message "The interface...

IMG_5007.jpeg

Resolved! STM32H7B0 DMA locked after first start

Hi,I use a STM32H7B0 100 pins and we would use a DMA to transfer data from 1 memory location to another.Therefore we use DMA1 stream 3 with a datasize of "Half word".What is very strange is that we cannot disable the option "Use Fifo" in stm32Cube.No...

OGhis by Senior
  • 1569 Views
  • 2 replies
  • 1 kudos

Resolved! Minimum Clock Speed, and enabling PSSI problem

Hello, I'm just evaluating the STM32H7R3Z8 for a new project. I'm having two issues, possibly with the STM32CubeMX, or maybe I'm just not understanding the part.1) No matter what I do, I cannot seem to enable PSSI. The combobox is grayed out with "Di...

pssi_problem.jpg
FA1234 by Associate III
  • 3002 Views
  • 5 replies
  • 4 kudos

Resolved! Debug problem with clone st-linkv2

Hi everyone!I use stm32f103c8t6 and clone st-linkv2 when i try to debug my codes with stmcubeide i had a lot of errors. Like connection error or debug path etc. I cant solve it. When i use MDK-ARM code is working but i cant get any data. Please help!

AnilKose by Associate II
  • 8660 Views
  • 14 replies
  • 21 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.