STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Motor speed estimation using TIM2 and TIM3 on STM32F407

I'm trying to connect an encoder with STM32F407VGT6. The encoder sends out A,B and Z pulses out. I can read both A-B and Z pulses using TIM2 and TIM3 respectively. Timer 2 is in encoder mode and TIM3 is in input PWM mode. I want to know if I'm correc...

zd9797 by Associate II
  • 2560 Views
  • 4 replies
  • 1 kudos

STM32G030 corrupting program on last minute write

I have a STM32G030K8 processor that needs to write some stuff to memory as soon as it detects that it will be losing power - always a bad time but I have to do this.Most of the time it seems to be doing this just fine but once in a while the processo...

Hendrik1 by Associate II
  • 5943 Views
  • 14 replies
  • 0 kudos

Resolved! EEPROM Emulation

A while ago a member of ST staff kindly helped me on this forum with adding EEPROM emulation to my design (at the time based on Nucleo-F401RE) by directing me to here....https://github.com/STMicroelectronics/STM32CubeF4/tree/master/Projects/STM32F4-D...

STM32H523 memory map

Hi,There seems to be an error in the reference manual RM0481 Version 2, page 264, table 48.In the circled image I believe this should be 0x08040000. Can you anyone please confirm my deductions?Kind Regards,Shane

KiwiNZ by Associate II
  • 1761 Views
  • 1 replies
  • 1 kudos

Resolved! Keeping peripherals in perpetual reset

Is it ok to keep unused peripherals in perpetual reset, by leaving their RCC_APBRSTR_*RST (or similar) bit set?Maybe differences in power consumption?This is not for a specific STM32 family.I'm just looking for advice by people with more experience, ...

SZano by Associate III
  • 2021 Views
  • 3 replies
  • 1 kudos

Resolved! Synchronize peripherals SAI & I2S output clocks

Heyho,I'm using a H733 with both SAI 1 and SAI 4 with SAI 1 as I2S clock master to get 8 synced audio channels.Audio clock comes from I2SCKIN, this is used for SAIs and I2S.Problem: because of the fixed oversampling ratio (256 or 512) of the SAI, I h...

LCE by Principal II
  • 4772 Views
  • 7 replies
  • 1 kudos

Nucleo-G431 onboard stlink can't work

Nucleo-G431 onboard stlink used normally before, but recently it suddenly couldn't be used, there was no response when connected to the computer with a USB cable, the computer could not detect the stlink (it can be determined that there is no problem...