STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! clock configuration issues when I use CAN

good morning. I want to implement a can loopback on my STM32H755, but when I enable FCAN1, then my clock can't resolve it issues and shows this for FDCAN in the picture below. how could I resolve this problem?  

Jad_0-1726221753821.png
Jad by Senior
  • 4316 Views
  • 9 replies
  • 0 kudos

ESP-PSRAM64H and STM32H743 QSPI mode

Hi,Is there any one success with ESP-PSRAM64H in memory mapped mode?We are able to read ID (0x9F) in spi mode. But when we read/write, it return 0xFF. We don't see EnableWrite command, does this chip has EnableWrite command?We also wanted to use thi...

Dat Tran by Senior II
  • 12624 Views
  • 15 replies
  • 0 kudos

STM32H743 SPI with CRC mode, acces to CRC from frame

Hello,- STM32H743-SPI2 Slave mode, RX onlyIf the frame has the format N x data + CRC, is it possible to receive the CRC and not just the result of comparing it with the calculated CRC?Receiving a CRC does not set the RXP bit and is not entered into t...

JarekC by Associate II
  • 2302 Views
  • 4 replies
  • 0 kudos

Issue with uart2 in STM32L073RZ nucleo board

I am using stm32l073rz neucleo board for my project.when i am trying to use uart 2 for my application, its not working as desired . That is when i connect A TTL module with the pins PA2 & PA3 on nucleo board i didn't get any output . But the same cod...

vijil by Associate
  • 1235 Views
  • 1 replies
  • 0 kudos