User Activity

We are using STM32H753I-EVAL2 evaluation board. We need to test SPI functionality of microcontroller. The board gives a provision to use CN6 & CN7 connector to do this. But the Samtec connector couldn't be connected with any jumping wires nor we coul...
Respected sir/madam,We are using STM32F411CEU6 blackpill board. When we try to put our code into the flash, it says it the memory is protected. Can you suggest possible solution to solve the issue?
Respected sir/madam,We are using STM32H753I-EVAL2 development board for testing STM32H753XIH6 microcontroller. We wanted to test SPI interface. But, the development board do not provide any provision for it.How can we test SPI functionality using the...
We are using STM32H743BIT6 microcontroller in our project. Which is the development board that we need to buy and use for this microcontroller for prototyping and development purpose? Can we use STM32H753I-EVAL2?
We are using a GPIO pin in STM32H743IIK6 microcontroller in open drain configuration. In datasheet, it is mentioned that Vol = 0.4V at IIO = 8mA and Vol = 1.3V at IIO = 20mA. What will be the Vol voltage at currents higher than 10mA? How does Vol var...