STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RCC AFIO

Posted on November 11, 2011 at 21:58Hello, i am trying to connect 4,3' TFT lCD with SSD1963 controller, and hit one problem original driver was for STM32F103, and function sound like this: RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOD  | RCC_APB2Perip...

SPI2 Not active

Posted on November 16, 2011 at 01:47#define SPI2_GPIO_CLK     RCC_APB2Periph_GPIOB #define SPI2_PORT      GPIOB #define SPI2_CLK                     RCC_APB1Periph_SPI2 #define SPI2_SCK_PIN               GPIO_Pin_13                #define SPI2_MISO...

lsc7718 by Associate
  • 1175 Views
  • 2 replies
  • 0 kudos

SPI Transfer Less Than 8-bits

Posted on November 15, 2011 at 22:57I have been reading the SPI documentation for the STM32F4 and it is unclear to me how things function if you have a transfer that is less than 8-bits.I have a piece of hardware that provides clock and data. There ...

ST32 and Linux

Posted on July 18, 2008 at 14:58ST32 and Linux #free-stm32-toolchain-for-linux

ettore by Associate II
  • 2570 Views
  • 5 replies
  • 0 kudos

Linker script: How to get the same size of BIN file?

Posted on November 15, 2011 at 12:33I need( from some reason) to get always the same size of bin file.I've tried to create other flash-section and fill it with some value.As last section I added following..  .added :  {    FILL(0xAB);    . = ALIGN(0...

lubos by Associate
  • 837 Views
  • 0 replies
  • 0 kudos

USART1 TX on PA9

Posted on November 12, 2011 at 19:15Hi, I would like to use the USART1 TX on pin PA9 but evan I remap usinf AF (alternate function), the USART1 doesn't transmit on PA9, it is like the USB OTG FS is keeping the pin. I would appreciate it a lot if som...

rdurand9 by Associate II
  • 1970 Views
  • 4 replies
  • 0 kudos

TIM2_IRQHandler never executes??!!

Posted on November 13, 2011 at 12:40Hello everyone,I have tried to use GPIO PortB, Pin 10 (which i believe can use AF TIM2_Channel 3) to capture PWM signals on my stm32f2.  I am using the standard peripheral lib. I am having issues with the TIM2_IRQ...

STM32F100 Timer-Clock

Posted on November 12, 2011 at 15:41Hello forum! I'm trying to get familiar with the timers in the STM32 but now I got stuck at a problem I can't solve, first here's the concerned function: void TIM4_Configuration(void) {   /* Compute the prescaler ...

General questions on STM32 programming paradigms

Posted on November 12, 2011 at 21:10I could not find any good document on internet about STM32 programming. Unfortunately, STM's own documents do not explain anything more than register functions. I will greatly appreciate if anyone could explain (o...

hate_pod by Associate
  • 2438 Views
  • 3 replies
  • 0 kudos