STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

when is SPI clock sent?

Posted on November 17, 2011 at 12:20Unfortunately I do not own an oscillope nor a logic analyzer to see this.I'm having some problem using the SPI controller to communicate with a sensor.I've managed to get some data, but not in a consistent way.In ...

salvatore by Associate II
  • 1712 Views
  • 2 replies
  • 0 kudos

FSMC problem with low address

Posted on November 17, 2011 at 15:38When try to access to SRAM through FSMC (SRAM example from IAR 6.1) I don't see any address on  ADDRESS 7:0. Only high frequancy (> 10 MHz) peaks and splashes. With ADDRESSes 20:8 all OK. With DATA BUS all OK.  Re...

milds by Associate II
  • 1288 Views
  • 2 replies
  • 0 kudos

STM32F4 Discovery AWD IRQ

Posted on November 15, 2011 at 14:41I have been able to successfully setup the ADC3 to set the SR, AWD flag when an input exceeds my threshold set.  What I am now looking to do is put the processor in sleep mode (via __WFI();) and then have it wake ...

How to unbrick?

Posted on November 15, 2011 at 00:41I previously posted[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32VLDiscovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32VLDiscovery/5V pin no longer supplies 5V; other problems too&FolderCTI...

mastyskal by Associate II
  • 2108 Views
  • 3 replies
  • 0 kudos

STM32F103ZE ARM FLY

Posted on November 17, 2011 at 12:06Excuse. What means PC 1 ADC123_IN10 in the table of gpio of stm32f103ze (arm fly).Means that the pin PC1 is the Pin of the ADC channel 10?

ADC_SoftwareStartConvCmd will enable external trigger?

Posted on November 17, 2011 at 10:13Hi all,I'm using StdPeriph lib and saw there is such code in stm32f10x_adc.c:#define CR2_EXTTRIG_SWSTART_Set     ((uint32_t)0x00500000)and /*** @brief Enables or disables the selected ADC software start conversion...

chaos by Associate
  • 816 Views
  • 0 replies
  • 0 kudos

Systick doesn't fires up as expected

Posted on November 15, 2011 at 14:39I programmed the systick timer in order to get 1ms delay but I seem to get a 10us delay instead.From the reference manual RM0008''The SysTick calibration value is set to 9000, which gives a reference time base of ...

salvatore by Associate II
  • 2131 Views
  • 4 replies
  • 0 kudos

SPI xfer using DMA

Posted on November 16, 2011 at 12:45Hi, I have my STM32F103RB connected to an ADC via SPI1. I read my ADC in two modes, in single shot mode I do SPI transfer in polling mode and all works well. In continuous mode I need to read data from ADC every 2...

mohith2 by Associate II
  • 1170 Views
  • 1 replies
  • 0 kudos

4 Input PWM and 4 output PWM

Posted on November 14, 2011 at 01:36The original post was too long to process during our migration. Please click on the attachment to read the original post.

csdominik by Associate III
  • 1802 Views
  • 2 replies
  • 0 kudos