2011-11-13 3:40 AM
Hello everyone,
I have tried to use GPIO PortB, Pin 10 (which i believe can use AF TIM2_Channel 3) to capture PWM signals on my stm32f2. I am using the standard peripheral lib. I am having issues with the TIM2_IRQHandler never being called/executed. Below is the code fragment to setup the GPIO, NVIC and TIM for PWMIN - GPIO_InitTypeDef GPIO_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; TIM_ICInitTypeDef TIM_ICInitStructure; RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; // Unclear on this setting GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOB, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOB, GPIO_PinSource10 , GPIO_AF_TIM2); NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); TIM_ICInitStructure.TIM_Channel = TIM_Channel_3; TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising; TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI; TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1; TIM_ICInitStructure.TIM_ICFilter = 0x0; TIM_PWMIConfig(TIM2, &TIM_ICInitStructure); TIM_SelectInputTrigger(TIM2, TIM_TS_TI2FP2); /* Select the slave Mode: Reset Mode */ TIM_SelectSlaveMode(TIM2, TIM_SlaveMode_Reset); TIM_SelectMasterSlaveMode(TIM2,TIM_MasterSlaveMode_Enable); /* TIM enable counter */ TIM_Cmd(TIM2, ENABLE); /* Enable the CC2 Interrupt Request */ TIM_ITConfig(TIM2, TIM_IT_CC2, ENABLE); The IRQ Handler is as below (note num_vists is a global variable and it never seems to increase ) - void TIM2_IRQHandler(void) { TIM_ClearFlag(PPM_TIM,TIM_FLAG_CC1); TIM_ClearFlag(PPM_TIM,TIM_FLAG_CC2); TIM_ClearFlag(PPM_TIM,TIM_FLAG_CC3); TIM_ClearFlag(PPM_TIM,TIM_FLAG_CC4); TIM_ClearITPendingBit(PPM_TIM, TIM_IT_CC2); TIM_ClearITPendingBit(PPM_TIM, TIM_IT_CC1); num_vists++;}Can anyone help me figure out what I have done wrong (i.e. why is the IRQ handler never visited).Regards,Srinath #stm32f2-pwm-input-capture2011-11-13 4:08 AM
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; // Unclear on this setting
Slew-rate control for pin. ie Drive Strength or SPEED. Not of consequence for an input. TIM_ICInitStructure.TIM_Channel = TIM_Channel_3;
TIM_SelectInputTrigger(TIM2, TIM_TS_TI2FP2);
/* Enable the CC2 Interrupt Request */
TIM_ITConfig(TIM2, TIM_IT_CC2, ENABLE);
What CHANNEL are you using/configuring?
2011-11-13 4:44 PM