STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Proper way to switch to HSE

Posted on April 05, 2012 at 18:43My application calls for using an external oscillator (not a crystal) as a clock source. To test this, I have an arbitrary function generator outputting a 50% duty cycle square wave of the expected clock rate. The MC...

shotaro by Associate II
  • 2282 Views
  • 3 replies
  • 0 kudos

STM32L151 jtag problem

Posted on April 08, 2012 at 16:18Hello ! I I start working with STM32L151  + Keil + ULINK2 ,  and  met a problem : after some code,  likely  it was  scommand  GPIOA->BSRRL=GPIO_BSRR_BS_2;processor stop the debugging, and a can not start  a new debu...

delay from two signals

Posted on April 03, 2012 at 20:12Hello at all, I have to mesaure the delay between 2 signals that I have in input to the microcontroller. I saw the example of the PWM input. I supposed to use an OR gate to have both front to the same pin but I think...

momede by Associate II
  • 2563 Views
  • 5 replies
  • 0 kudos

ST32F217 with STE100P. How to configure PHY address?

Posted on April 04, 2012 at 07:04STE100P how to set PHY address?Hello. Im trying to using an STE100P PHY ethernet chip (with ST32F217 MCU). In the datasheet for STE100P i see an description for bits 7~3 PAD4:0 in PR20- XMC, XCVR Mode control registe...

andrey23 by Associate II
  • 2282 Views
  • 4 replies
  • 0 kudos

Ethernet PHY DP83848CVV

Posted on April 04, 2012 at 13:55Hello, I want to use DP83848CVV as Ethenet PHY with STM32F207ZET6 in RMII mode. In Schematics (STM3220G_EVAL),there is some resistor of 51 Ohm in between of  signals (RMII_REF_CLK,RMII_TX_EN,RMII_TX_D0,RMII_TX_D1,RMI...

migrating from Atollic to IAR

Posted on April 05, 2012 at 07:39Hello, reasently i changed ide to iar and i getting strange problems: i have working code developed in atollic and tested on my discovery boards, but then i use same code on IAR, it just doesn't work. Like touchscre...

linas2 by Associate II
  • 1658 Views
  • 3 replies
  • 0 kudos

STM32F207

Posted on April 04, 2012 at 12:16Hello, I would like to download a C compiler for STM32F207. Where I could find it? I was searching through the forum, but without success. #stm32f207 #c/c++-compiler

dove457 by Associate
  • 1454 Views
  • 2 replies
  • 0 kudos

RTC calibration

Posted on March 29, 2012 at 07:42Hi all,I wanted to know is there any software workaround to compensate for negative ppm values.I am using STM32F100V8 controller. According to the rtc digital calibration manual(attached) you can only subtract the cy...