cancel
Showing results for 
Search instead for 
Did you mean: 

ST32F217 with STE100P. How to configure PHY address?

andrey23
Associate II
Posted on April 04, 2012 at 07:04

STE100P how to set PHY address?

Hello. Im trying to using an STE100P PHY ethernet chip (with ST32F217 MCU). 

In the datasheet for STE100P i see an description for bits 7~3 PAD4:0 in PR20- XMC, XCVR Mode control register :

(page 15 of datasheet 

http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/DATASHEET/CD00001918.pdf

 )

PHY Address [4:0]:

The values of the PAD[4:0] pins are latched to this register at 

power-up/reset. The first PHY address bit transmitted or 

received is the MSB of the address (bit 4). A station 

management entity connected to multiple PHY entities must 

know the appropriate address of each PHY. A PHY address of 

<00000> that is latched in to the part at power-up/reset will 

cause the Isolate bit of the PR0 (bit 10, register address 00h) 

to be set. 

After power up/reset the only way to enable or disable isolate 

mode is to set or clear the Isolate bit (bit 10) PR0. After power 

up/reset writing <00000> to bits [4:0] of this register will not 

cause the part to enter isolate mode.

But i cant see any of PAD[4:0] pins in chip pins (

http://circuits.datasheetdir.com/204/STE100P-pinout.jpg

). 

How can i set PHY address for STE100P?

#phy #ste100p
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
amin23
Associate II
Posted on April 05, 2012 at 18:47

Hello,

Please refer to the following pages:

page 5: Table 2. Pin Description (continued)

page 15: Table 5. Register Descriptions (continued)

ledr10 --> PAD4

ledtr  --> PAD3

ledl   --> PAD2

ledc   --> PAD1

leds   --> PAD0

andrey23
Associate II
Posted on April 06, 2012 at 06:45

Thank you! but how can i pull up or pull down LED pins, how LEDs will work after that?

andrey23
Associate II
Posted on April 06, 2012 at 08:12

Thank you! You save my project)