STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

spi error send slave

Posted on April 11, 2012 at 19:48Hi, I got two different devices with the microcontroler STM32F103RB which I'm trying to comunicate between them using the SPI protocol. The element A, is the master : The element B, is the slave : When I send from A(...

bfeixas by Associate II
  • 1891 Views
  • 2 replies
  • 0 kudos

STM32F10x execute application from SD card

Posted on April 11, 2012 at 21:40Hi everybody, I'm new in STM32/Cortex M3. Commonly I create an application then write to chip's flash. Now, if I want to create an application stored in SD card then run that application. What the way for MCU do that...

Tftp server with FreeRTOS (stm32f4)

Posted on April 11, 2012 at 16:12Hi, I downloaded the package : LwIP TCP/IP stack demonstration for STM32F4x7 microcontrollers. I tested different programs : udp_serverclient, tftp_server without RTOS and udptcp_echo_server with RTOS. And now I sear...

Hard fault from waking up from low-power sleep

Posted on April 11, 2012 at 02:22I seem to run into a lot of issues! I'm trying to get my STM32L Discovery board to wake up from low-power sleep with the Flash turned off. I'm using the User button (tied to PA0) to wake it up as an external interrup...

shotaro by Associate II
  • 911 Views
  • 1 replies
  • 0 kudos

No output from DAC @STM32F103VExx

Posted on April 10, 2012 at 17:50Hi,I am a university undergrad and I am designing a Digital storage oscilloscope. I need the micro controller's DAC output for DC voltage. I have seen the sample code and I know how to setup the timer, link the DMA t...

rajan2 by Associate II
  • 2244 Views
  • 3 replies
  • 0 kudos

adc

Posted on April 01, 2012 at 23:12in my project, i must generate a sinusoidal wave and i have to receive this wave by ADC. this signal is a response harmonic of a filter. so i want to calculate the gain and the phase shift but i don't know how. can i...

SDIO/DMA and Filesystem

Posted on March 29, 2012 at 21:49Hi all, i'm sorry if this has been discuss before, but from reading posts i'm still some what unclear, thus my post.Right here goes :)Has anyone implemented reliably SDIO using DMA along with say FatFS file system ? ...

stm32F100 RX

Posted on March 20, 2012 at 17:28hi can any one help me this code seems to be right but i dont know what' the matter with Rx FAILED LED turn always on !!!???#include ''stm32f10x.h''#include ''stm32f10x_rcc.h''#include ''stm32f10x_usart.h'' #include ...