STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F410: ITRx "reserved"?

Hi guys,can someone please explain the internal trigger connections for the stm32f410 controllers to me?According to the referance manual (RM0401, see below) only TIM1 and TIM5 can be configured as slave timers with just ONE possible internal trigger...

ITR.png

Powering STM through USB-C port

Hi,I want to power a STM32Ux based board using USB-C port. I am required to use two numbers of  a Type-A to USB-C type of cable and also it should support USB-C to USB-C type of cable in OR ring. Max load current of the board is less 1.5A. I am looki...

SKCL-1 by Associate II
  • 1896 Views
  • 3 replies
  • 0 kudos

Resolved! Is there IR TV remote project example with TIM16 and TIM17 ?

Hello, I am looking for very old STM32CubeIDE project example for IR TV remote control to see how TIM16 and TIM17 are set up and controlled.I am not interested in manuals and instructions: better one time to see then read about it 100 time and not ge...

GS2 by Senior II
  • 3026 Views
  • 7 replies
  • 1 kudos

USB only working in debug mode

Hi  I am working on an STM32L433 using STM32IDE. When running in debug mode, the USB CDC is recognized when plugging in the cable (into Windows 10 and 11) . But when I compile as release mode the USB isn't recognized . I am using the HAL for USB . An...

STM32F469I-Disco board all dimensions

Dear Team,We are using the ST32F469I-DISCO development board and are currently designing an extension board to pair with it. For proper alignment, we need the precise dimensions of the Arduino headers, the expansion headers, and the mounting holes. T...

Its1 by Associate
  • 1248 Views
  • 2 replies
  • 1 kudos

STM32f401rct6 rcc cr register

Hi, noob here.I have a problem with the cr register, that's when I open the hse and Pll bite the ready register always been 0, if I need another operation? the output from the cr rigister is always value: 1000000010101101110000011. Thanks for your ti...

Shevshy by Associate
  • 880 Views
  • 1 replies
  • 0 kudos