STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! FDCAN Configurations to Transmit Data in Classic mode

Devkit - NUCLEO-H563ZI IDE - STM32CubeIDE Version: 1.16.1 Build: 22882_20240916_0822 (UTC) Details - Trying to create a sample program for FDCAN in which the program transmits the data using the CAN protocol. I have tried different methods but was no...

mayank__ by Associate II
  • 5244 Views
  • 8 replies
  • 0 kudos

Resolved! Output voltage

Wanted to confirm if the input/output voltage is 3.3V or 5V depending on the I/O structure of my pin . I scoped a PWM signal with the board connected to the PC and on the dedicated pin I see the signal in  mV. I would like to send a higher voltage th...

Marrkinho by Associate II
  • 5324 Views
  • 2 replies
  • 3 kudos

Resolved! ST-Link driver issue

Hi All,I would need the link to download the ST-Link driver 2.1.0.0 from 08/06/2017.The latest one is interrupting the connection to board randomly every couple of seconds.I cannot find any link to the former ST-Link drivers, so please provide me the...

Sebdee by Associate II
  • 2310 Views
  • 4 replies
  • 0 kudos

Two Resets Required for STM32G474

Hello All, I'm having a problem with an STM32G474 on a custom board. Overview of FaultFirst, weird behavior of the IWDG was observed. A hard fault was generated intentionally after 10 seconds of run time and no reset behavior was observed. Then, a wh...

RyanColeman_0-1729211736247.png RyanColeman_1-1729211747965.png

Read Systick Timer Value Directly for 1ms Timebase

Hi, I am working on a project on the STM32H730 that runs a high priority audio interrupt thread as well as a lower priority asynchronous loop for user interface processing and a 1ms SysTick interrupt for user interface processes that need some accura...

EPala.2 by Senior
  • 8162 Views
  • 17 replies
  • 0 kudos

Resolved! How to enable/disable Flash Write Protection?

Hi guys,I am read the example "STM32Cube_FW_F1_V1.8.4\Projects\STM32F103RB-Nucleo\Examples\FLASH\FLASH_WriteProtection", and want to rewrite it on my board.my code is as follows:  HAL_FLASH_Unlock(); HAL_FLASH_OB_Unlock(); HAL_FLASHEx_OBGetCo...

Junde by Senior III
  • 6976 Views
  • 3 replies
  • 0 kudos

Resolved! Problem with I2C4 on STM32H745I-Disk

I have two codes, one only with the I2C4 communication working and the other code besides the I2C has the display but in this one the I2C communication does not work, what could be happening?With a logic analyzer I can see that in both codes the cloc...