Skip to main content
Associate
July 10, 2024
Solved

Baud rate of 4Mbps

  • July 10, 2024
  • 3 replies
  • 1720 views

Hello everybody,

This is my first post hope i wll get the answer.

I am building a spectrometer for which i am using a stm32f401re board and i need to sample the data coming from a sensor at 250kHz which nearly gives a data rate of nearly 4Mbps so do i need to use 4Mbps baud rate to read that and if so how to achieve such higher baud rates.

Thank you.

This topic has been closed for replies.
Best answer by AScha.3

From ds:

AScha3_0-1720601963254.png

 

 

So whats the problem?

3 replies

mƎALLEm
ST Technical Moderator
July 10, 2024

Hello and welcome to the community.


i need to sample the data coming from a sensor at 250kHz which nearly gives a data rate of nearly 4Mbps

Not clear! Is it over a protocol communication? which one?

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
000harshaAuthor
Associate
July 10, 2024

Yes it is over UART

AScha.3
AScha.3Best answer
Super User
July 10, 2024

From ds:

AScha3_0-1720601963254.png

 

 

So whats the problem?

If you feel a post has answered your question, please click on " Best Answer ".