STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is it possible to use i2c in a full duplex mode?

Posted on September 07, 2012 at 08:09Hi! all,Is it possible to use i2c of stm32l152rbt6 in a full duplex mode? if so can you post/send me the relevant code for that.thanks,  #i2c-in-a-full-duplex-mode #i2c-fundamentals

STM32F103 Download Hex File Using Command Line

Posted on September 07, 2012 at 09:12Hello,I want to download hex file to STM32F103 using STMFlashLoader.exe. But I haven't been successul yet. Do you have sample command with work STM32F103? It's very useful for me to understand command line.Thank ...

MB1034B STM32F0DISCOVERY problem on UART1 PA10

Posted on September 07, 2012 at 09:01I'm using STM32F0DISCOVERYI can't receive any char on UART, no interrrupt!Here my initialization:&sharpdefine RCC_PORT_RX RCC_AHBPeriph_GPIOA&sharpdefine GPIO_PORT_RX GPIOA&sharpdefine GPIO_PIN_RX GPIO_Pin_10&s...

MicroXplorer as Eclipse plugin with Linux

Posted on May 31, 2012 at 12:27Hi,does anybody use the MicroXplorer Eclipse plugin with Linux and Eclipse 3.7?Here it either crashes Eclipse or I can't choose an MCU.Moritz #microxplorer-ubuntu64-crashes

Moritz M by Associate II
  • 1818 Views
  • 3 replies
  • 0 kudos

TIM_ICPolarity_BothEdge not available for most timers???

Posted on June 06, 2012 at 07:36Hi. I need to read a digital signal coming into an STM32F100. Timing how long the signal is in a low state and also knowing if the counter overflowed would give me the two pieces of information I need (value of the da...

laurie by Associate II
  • 1926 Views
  • 3 replies
  • 0 kudos

SDIO + DMA + CRC

Posted on September 06, 2012 at 10:49ello,I sometimes have problems with blocks which are written completely wrong onto the sd-card. Workaround: actually I check the written data again by reading the same block from SD-card and check the both buffer...

Problem with two consecutive _SdRead()

Posted on September 03, 2012 at 18:08 Hi, I am using the software example 'MassStorage' , the IAR compiler and the STM32F103ZE kickstart board for development. I wanted to add some functionality which requires consecutives reads from ...

colsman by Associate II
  • 1344 Views
  • 4 replies
  • 0 kudos

STM32F4 not passing EV6 on I2C

Posted on September 06, 2012 at 07:13I'm having some difficulty communicating with a TI INA219 using an STM32F407VE and I2C1 on PB7 and PB8. Sending data seems to work just fine, but receiving it does not. Namely, my EV6 (I2C_EVENT_MASTER_RECEIVER_M...

Help interpreting USB OTG docs for stm32f1xx

Posted on September 05, 2012 at 16:30Hi all! The software design process we use requires that every piece of code is heavily tagged with references to the original programming manuals. Sometimes these tags are added during code reviews, etc. The que...

ashibakov by Associate II
  • 2763 Views
  • 6 replies
  • 0 kudos