Posted on May 17, 2011 at 14:19Two remarks 1) Now I have three step motors that I configure each to work 20 Hz, which is 6 [rpm], which is very slow. I understand that in that case I dont have to use TIMx_RCR, and I even may monitor each pulse with ...
Posted on May 17, 2011 at 14:04 Hello I have an STM3210C_EVAL board I have a strange problem 1. I am working with some device that is connected with RS485/RS232 converter halfduplex to USART2 of the EVAL board 2. When I configure the USRAT2 with 384...