cancel
Showing results for 
Search instead for 
Did you mean: 

CPLD configuration using STM32F101

infoinfo977
Associate
Posted on December 31, 2010 at 10:38

CPLD configuration using STM32F101

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Andrew Neil
Super User
Posted on May 17, 2011 at 14:20

''Is it possible?''

Yes, of course it is possible - many PLD manufacturers have app notes showing how to do it with processors far less capable than an STM32!

''Is there some libraries for JTAG master?''

 

The tricky part is not the JTAG - that's just a matter lf bit-banging a few pins;

The information you really need is the specific protocol/process required for updating the particular CPLD that you are actually using. For that, of course, you will need to refer to documentation from the CPLD manufacturer...
A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.