STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F10x peripheral driver bug

Posted on September 09, 2012 at 16:31 I found the following bug. I have a 16MHz crystal on my board design. I use the STM32F103RB uC with Atollic True Studio Lite 3.2. The stm32f10x.h advises me to set theHSE_VALUE according to my crys...

rigomate by Associate II
  • 2357 Views
  • 5 replies
  • 0 kudos

STM32F103RE: ISP bootloader doesn't work correctly

Posted on September 05, 2012 at 15:58Hello, I just started a new project with the F103RE controller. Opposed to the F103RB I have used before, the ISP bootloader in this chip simply does not work. Though it is obviously running correctly (verified b...

tilmann by Associate III
  • 6153 Views
  • 19 replies
  • 0 kudos

Timer Duration Count With Interrupt

Posted on September 10, 2012 at 12:26A fairly basic thing to do which I am struggling to find any precise examples for.I want to be able to setup a Comms timeout - specifically on an SPI connection whereby if  I don't get a response to a command I s...

dclark9 by Associate II
  • 2963 Views
  • 5 replies
  • 0 kudos

STM32F4 USB Host HS for MSC

Posted on May 26, 2012 at 17:08hi all i try to work with usb host hs for msc. but no answer ! my program in this instruction looped :     do     {       status = USBH_MSC_Read10(&USB_OTG_Core, buff, sector, 512*count);       USBH_MSC_HandleBOTXfer(&...

jt1355 by Associate
  • 1836 Views
  • 4 replies
  • 0 kudos

SYSTICK is really funky - I think

Posted on September 10, 2012 at 09:25In my application I set up SysTick with: SysTick_Config(SystemCoreClock / 1000);to generate a 1ms interrupt.I got some weird timing anomalies and eventually used a timer interrupt to generate 1ms interrupts using...

carl2399 by Associate III
  • 1075 Views
  • 1 replies
  • 0 kudos

Internal temperature sensor

Posted on July 02, 2011 at 20:18Hello.I'm trying to use the internal temperature sensor, but I can't understand the reference manual formula:  Temp = ((V25 - Vsense) / Avg_slope) + 25).In the product datasheet, it says V25 is 1.41 V and Avg_slope is...

Recover ST-LINK firmware

Posted on September 07, 2012 at 14:29Hi, I would like to know if its posible to restore st-link firmware on the STM32F103C8. I have 2 boards and I tried to program it to play a little with USB. Can I restore it? How? Thanks in advance.

rmarku by Associate
  • 1342 Views
  • 1 replies
  • 0 kudos

HSERDY bit is always 0

Posted on September 08, 2012 at 14:48Hi guys, I have a board from hardware guys who told me they had tested this board and everything is fine including SPI1. But I cannot let my SPI1 working because status register bit TXE is always 0. From the spec...

UART4 Rx

Posted on September 10, 2012 at 04:03Hello every1, few days ago i had a problem with uart tx and nw i have solved that problem. so my tx is working fine now. my rx is working too but very slow and gets junk values. below is my code. int main(void) {...

vivek2 by Associate II
  • 2159 Views
  • 4 replies
  • 0 kudos

how to update TIM_Period when timer i running

Posted on September 09, 2012 at 21:55Hi I need to be able to update the Period for a timer (TIM3) I though it was simple, but no.I have tried :else if(TIM_GetITStatus(TIM3, TIM_IT_Update) != RESET){ ledTimeBaseStructure.TIM_Period = newValue; TIM_Ti...

spa23 by Associate III
  • 795 Views
  • 1 replies
  • 0 kudos