STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

use SWD connection on discoveryL board and J-link

Posted on January 11, 2013 at 17:43Hi,For the moment I'am using the STM32l discovery card (stm32l152R8 chip). I write a programm to toggle led and i donwload it with st-link V2 which is integratted on the board.It's working. Now I would like to conn...

gfoujanet by Associate II
  • 2227 Views
  • 3 replies
  • 0 kudos

connecting lcd to stm32f4 module

Posted on December 16, 2011 at 05:30Just starting out with the eval board, and my question is what pins are used to connect an lcd to the board? The only info on the data sheet is it uses fsmc function for lcd interfacing. This does not explain whic...

jara8462 by Associate II
  • 2831 Views
  • 4 replies
  • 0 kudos

BASIC

Posted on March 10, 2009 at 09:48BASIC

ccowdery9 by Associate III
  • 2115 Views
  • 5 replies
  • 0 kudos

Question on UART and HSE setting on Keli

Posted on January 12, 2013 at 08:08I am writing the program on Usart but the program is not function well. Here is the program:&sharpinclude <STM32F4xx.h>&sharpinclude <stdio.h>&sharpinclude ''stm32f4xx_gpio.h''&sharpinclude ''stm32f4xx_rcc.h''&shar...

jjyy1991 by Associate II
  • 2206 Views
  • 6 replies
  • 0 kudos

Triple ADC with DMA data misalignment

Posted on January 07, 2013 at 11:14Hello, I have works on triple ADC conversion using DMA and it works, but I don't understand why I have some misalignment. I use STM32F4-Discovery borad. ADC config is : ADC1 :            ADC2:                ADC3: ...

yayi by Associate II
  • 3303 Views
  • 5 replies
  • 0 kudos

STM32F4 MPU

Posted on January 11, 2013 at 08:43Where is the documentation for STM32F4's MPU.  The datasheet only briefly mentions it and it's non-existent in the reference manual.  The Standard Peripheral Library 1.0.1 only has some CMSIS code but that's it.  A...

mfranklin by Associate III
  • 1340 Views
  • 2 replies
  • 0 kudos

Disabling JTAG on STM32L151

Posted on May 05, 2012 at 18:46I'm using STM32L151R8. I have SPI slave on SPI1 pins PB3-PB5 and CS on PA15. The SPI doesn't seem to work and i need to double check the warning about disabling the JTAG pins.But STM32L151xx reference manual has funny ...

STM3240G-EVAL & SRAM

Posted on January 03, 2013 at 20:25Hi. I know that the evaluation board have ~192k of ram , and 16mbit of external RAM, my question is how can i use the 16mbit of RAM,how do i ''tag'' variables to be allocated on the external RAM ? Thanks Michael