User Activity

Hi,I have found some questions and discussions with similar topic, but no answer seems to apply to my case. I have an STM32WB55 Nucleo Pack, and I cannot manage to load any of the BLE stack binaries provided with the STM32Cube_FW_WB_V1.16.0 into my d...
Hi, am using the STM32WB55 Nucleo board. My problem is, currently Iseem not to have a CPU2 wireless stack loaded and I fail to load filestm32wb5x_BLE_Stack_full_fw.bin loaded into the Flash. I am using theSTM32CubeProgrammer V2.12.0. When selecting o...
Posted on November 22, 2017 at 12:57Hi,I have problems with ethernet (using the HAL library 1.8.0) on the STM32F756ZG.If I place the DMA buffers in the DTCM (0x20000000-0x2000ffff), it works fine. If I place the DMA buffer anywhere else (SRAM1, SRAM...
Posted on May 08, 2017 at 13:45Hi,i want to report a bug in the library 'STM32F2xx_AN3390_FW_V1.0.0', which can cause the loss of user data.On startup, the library checks the status of the two Flash pages. If one page is marked 'valid' and the other...
Posted on March 30, 2016 at 18:25Hi, I am looking how to save a few bytes in RAM. I am using the standard peripheral lib, and included in stm32f10x_rcc.c, stm32f2xx_rcc.c and stm32l1xx_rcc.c, I found some static constant arrays (PLLMulTable, APBAHBP...
Kudos from