User Activity

Posted on November 10, 2011 at 07:35the ctrl registers remain at reset values but idr 0 an 1 goto low(0). is there something wrong with my source? // // // //STM32 BUTTON TEST //by T. Herring tre2020067@gmail.com // /////////////////////////////////...
Posted on November 10, 2011 at 07:27the ctrl registers remain at reset values but idr 0 an 1 goto low(0). is there something wrong with my source? // // // //STM32 BUTTON TEST //by T. Herring tre2020067@gmail.com // /////////////////////////////////...
Posted on October 17, 2011 at 21:30can i but 9 bits in the SPI Tx buffer configured in 8bit mode and have it still clock out all 9 bits???
Posted on October 01, 2011 at 21:35I closed the old thread for this lcd so that others my search for this thread more easily in the future. okay, so i have a ST32F103VET6 and a ili9325 based lcd im trying to control using FSMC. the code compiles and...
Posted on September 26, 2011 at 07:23im trying to interface a ILI9325 and im not 100% understanding how the write function works.the function was ripped from a driver file for the ILI9325 and the ports PC are used to control the control lines.why is...