STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

F4 DMA to SDIO NDTR Problem

Posted on January 26, 2013 at 01:26Somehow I can not reply to https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https%3a%2f%2fmy%2est%2ecom%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fDMA%20to...

picguy2 by Associate II
  • 656 Views
  • 0 replies
  • 0 kudos

STM32F051 EEPRom emulation (AN4061)

Posted on January 25, 2013 at 17:12Hi All, According to the apps note AN4061, a page erase should only occur when one page is full. For instance, after the first run and the memory is formatted, page0 is marked as VALID_PAGE, and page1 is marked as...

Re-program Product

Posted on January 25, 2013 at 06:39Dear All, I bought any product that contained STM32F103C8T6 48-pin mcu. I try to re-program it with my own hex file using Flash Loader Demonstrator and it can be wrote and verified correctly but the application can...

zamzoni by Associate II
  • 2208 Views
  • 5 replies
  • 0 kudos

howto get tim_16 Frequ. to PB8

Posted on January 24, 2013 at 21:54Hello, My problem is that I don't get the Frequency produced by Timer 16  seen on PB8. Somebody can have a look at the code and tell me what's missing or wrong.  static void setup_Timer16(void) {     TIM_OCInitType...

jgnoss by Associate III
  • 1129 Views
  • 2 replies
  • 0 kudos

timer delay deviation with stm32f051

Posted on January 24, 2013 at 16:18Hello, I'am struggeling with a timer delay function, I've made a delay_us() function with help of timer14 However, when I have a delay which is close to zero I have lots of deviation. Here is my initialisation:#de...

evert2 by Associate II
  • 1670 Views
  • 3 replies
  • 0 kudos

Recommended Oscillator for STM32F407

Posted on January 25, 2013 at 01:05I have designed a custom board around STM32F407VET.  I am using 8 MHz external oscillator (ABRACON ABLS-8.000MHZ-B2-T) with 22 pf load capacitors (CL) and 220 ohm REXT.  When I probe OSC_IN or OSC_OUT pins using lo...

STM32 FAST DATA COMPRESSION AND LOW MEMORY FOOTPRINT

Posted on January 24, 2013 at 17:03Hello,I need to design a system which will compress a data with rate of 1000:1 minimum in the range of  determined time.I want to compress data (tera bytes to gigabytes) and to save to SD card.I searched about open...

irmakci by Associate II
  • 4755 Views
  • 3 replies
  • 0 kudos

STM32F4discovery measuring a pulse duration

Posted on January 22, 2013 at 16:53 I am having some trouble setting up an external pulse duration measurement on a Timer. Ideally I'd like to capture the duration of just the first incidence of a pulse on the desired pin, but that could require ...