User Activity

Feature request to STM32 CubeIDE.ST, please add a possibility to add user explanation text to peripheral configurations. It is neccessary because the configuration, especially numbers, are not always self-explaning. A text field where to write explan...
I don't fully understand one thing with STM32L552 which has no SMPS: Does decreasing the VDD from 3.3V to say 1.8V reduce it's power consumption?All the measurements in datasheet and in AN5213 are done for operation ranges and in SMPS modes I see tha...
Posted on July 01, 2018 at 10:43Can anybody tell me if the VL53L1X device address is stored in volatile or non-volatile memory? I have multiple sensors in application and i don't want to have reset/shudown lines for every single one of them just for...
Posted on October 01, 2015 at 08:16  The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on August 25, 2015 at 20:45I am thinking of building several ''shields'' with GSM, GPS, LCD, MicroUSB and MicroSD connectors to stack up on the STM32F401 Nucleo board (by the dual row connectors, not Arduino) but i'm worried about the signal ...
Kudos from
Kudos given to