User Activity

Posted on January 09, 2012 at 04:49The readme.txt for Flash Loader V2.4.0 provides information as below? Last version V2.4.0 - 07/18/2011 Supported Microsoft OS:  Windows 98SE, 2000, XP, Vista, Seven.But Flash Loader can't run on my PC (OS: Windows...
Posted on November 21, 2011 at 14:27I test the USB HOST HID example with STM32F207,a keyboard is connected to USB FS port.When the program is executed, the keyboard can be recognized by STM32F207,and LCD display message:HID device:keybd,but it doesn...