STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI DMA with ADS1256 on STM32f103RB

Posted on January 29, 2013 at 18:04Hi everybody,I wanna know if its possible to use DMA SPI for drive the ADS1256 or similar where I can ''stop'' the tranfer to wait until the time to convert T6 (Delay from last SCLK edge for DIN to first SCLK) of t...

0690X00000602nZQAQ.jpg
felipe by Associate II
  • 2594 Views
  • 5 replies
  • 0 kudos

stm32f103zet + fsmc+ssd1963

Posted on February 01, 2013 at 08:38The original post was too long to process during our migration. Please click on the attachment to read the original post.

STM32L: does it use NOR Flash?

Posted on January 24, 2013 at 07:53I've noticed that STM32L initializes Flash to 00 instead of FF.  Yes, it has an EEPROM section that can be used for 4KB of NV data storage, which is great.  I suspect that is actually NOR Flash as well.Anyway, if S...

jpnorair2 by Associate II
  • 2140 Views
  • 4 replies
  • 0 kudos

gdb SIGTRAP

Posted on January 31, 2013 at 13:38 Hi, I have a problem for the second time, I don't know why but hardware breakpoint, sometimes, still in stm and I can't delete it. I use OpenOCD 0.6.1 and gdb This is my gdb log : ...

Linker error when compiling with CodeSourcery

Posted on January 31, 2013 at 13:06Trying to get a linux toolchain up and running to eventually program an STM32L Discovery board.  I have Code Sourcery CodeBench Lite set up in a folder and a Make script set up to build it all.  Right now it's just...

Read Out Protect - Only a section?

Posted on January 31, 2013 at 13:48Hi all,Is it possible to read out protect only one specific area of flash?I want to use a bootloader that can program both encrypted and un-encrypted programs.I need to protect the bootloader from being read so un-...

mwp by Senior
  • 1504 Views
  • 3 replies
  • 0 kudos

Read out Start-Up RAM values

Posted on October 12, 2012 at 11:28Hey there, I am pretty new to micrcontrollers and such. I recently bought a STM32VL Discovery, which I am programming with CoCoox IDE. My goal is to read out the start-up values of internal RAM. By start-up values ...

an by Associate II
  • 9950 Views
  • 27 replies
  • 0 kudos

DAC output not working

Posted on September 05, 2012 at 04:38Hi All, I had the DAC working using DMA to out put a sinewave continuously and it seems to have stopped working when I tried to change which timer I triggered off. After changing the timer configuration back it s...

Dual Quadrature encoders

Posted on January 31, 2013 at 08:04I am trying to read a paid of quadrature encoders, I have managed to get one to read using code copied from this forum but I have been un able to read the second one, I have tried it on different timers (1,3,4) and...

pisaacs9 by Associate II
  • 1253 Views
  • 1 replies
  • 0 kudos

Building 0s/03 doubles timer speed?

Posted on January 24, 2013 at 14:48Hi all,My TIM3 timer is setup to run at 10Khz which it does when i compile with -O0.When i compile with -03 or -Os, the timer speed increases to 20khz.All other build configs (gcc, linker, libs, etc) stay the same....

mwp by Senior
  • 2677 Views
  • 7 replies
  • 0 kudos