STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! THE DCMI 4 WORD FIFO IN STM3U5

Hello, STM32 community,I’m currently working with the STM32U5 and using the DCMI (Digital Camera Interface) to interface with a ADC Module which has a pixel clock and outputs 14-bit parallel data. While I understand that the DCMI supports extended da...

JP.4 by Associate II
  • 1830 Views
  • 2 replies
  • 0 kudos

RTC internal wake-up doesn't wake-up STM32U5

Hello,I have my STM32U575 set to wake-up from standby-mode by the reset button of the Nucleo-U575ZI-Q. Furthermore I want the MCU to wake-up periodically triggered by the RTC. The sample code below just makes the reset button work but the RTC doesn't...

Resolved! shutting down "spare" Cortex-M4

I've taken over this project that is using the STM32h755 CPU. The software is not currently using the Cortex-M4 processor inside the chip. I'm reworking the software so that it will be able to use it sometime in the future. But, until then, I was hop...

Resolved! STM32F429 ADC problem

I am currently using STM32CubeIDE and want to input an external sine wave. The signal has a voltage of 2.6V and a frequency of 10kHz, and I am using DMA + TIM + ADC. The following is the screenshot of my settings. Currently, I can only capture the pe...

tasabao_2-1729413430489.png tasabao_1-1729413412132.png tasabao_0-1729413380782.png tasabao_3-1729413475914.png
tasabao by Associate III
  • 5866 Views
  • 11 replies
  • 1 kudos

Timer input capture into DMA buffer how get position ?

HI, i use CC2 on TIM1 set as input capture measuring pulse period and store in array   /* USER CODE BEGIN TIM1_Init 1 */ LL_DMA_SetPeriphAddress(DMA1, LL_DMA_CHANNEL_3, (uint32_t)&TIM1->CCR2); LL_DMA_SetMemoryAddress(DMA1, LL_DMA_CHANNEL_3, (uint...

MM..1 by Chief III
  • 1792 Views
  • 3 replies
  • 0 kudos

STM32U5A5QJ Part Selection Clarification

Hi,We are currently in the process of selecting components for our project, and we have identified the STM32U5A5QJ9 (STM32U5A5QJ), foot-print size UFBGA 132 7x7x0.6 P 0.5 mm) microcontroller as a potential candidate. However, upon reviewing the datas...