STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Flash Read and Write Problem

Posted on March 19, 2013 at 10:40Hi,      I want to display 2 parameters(ID and BD) value on seven segment display. The values will be dynamically changed, so every time I want to write these 2 byte of values on FLASH memory and every power ON or Sy...

ss2 by Associate II
  • 6514 Views
  • 11 replies
  • 0 kudos

STM32F3Discovery, replaced MCU with STM32F407VGT6

Posted on March 21, 2013 at 00:23Hi,I have a STM32F3Discovery eval. board which I used to build an IMU controlled by a computer through Graphical User Interface. This is an excellent board (9 Degrees of Freedom) and it is a good way to start.I have ...

ebader18 by Associate
  • 1516 Views
  • 2 replies
  • 0 kudos

problem on 3V3 IO to drive 5V chipset with SPI

Posted on March 19, 2013 at 16:07Dear everyone,     I met a problem when I try to use the SPI (3.3V) to drive the meganetic isolation ADum2400 which is powered by 5V.The SPI pin are remapped to SPI3 (PC10, PC11, PC12) and the CS pin are remapped to ...

xinjin by Associate II
  • 3665 Views
  • 5 replies
  • 0 kudos

I2C witch PCF8574P (keypad 4x4)

Posted on March 20, 2013 at 20:14Hi,I would like to control keypad through PCF8574, but some problemsare occurring like (reading only one time), and receiving 'ack' even disabled.''http://www.nxp.com/documents/data_sheet/PCF8574.pdf''(see de picture...

0690X0000060Mm1QAE.gif
esiqueira by Associate II
  • 1642 Views
  • 1 replies
  • 0 kudos

STM32L-Discovery st-flash problem (error)

Posted on March 20, 2013 at 19:24Hello,I have a problem while trying to flash a *.bin file into my STM32L-Discovery board.The following error is shown:./flash/st-flash write /Users/jaspervandenakker/Documents/stm32l-discovery-projects/workspace/STM3...

UART and PLM ST7540 on cortexM0

Posted on March 20, 2013 at 16:53Hi guys,i'm learning about the st7540 PLM device.My hardware configuration is the seguent:STM32F0Discovery board and two EVALST7540-2 (st7540 transceiver).Microcontroller--->St7540transceiver--->220V--->St7540trancei...

pietro2 by Associate II
  • 635 Views
  • 1 replies
  • 0 kudos

Interrupt enabling/disabling

Posted on March 18, 2013 at 19:15Hello,please look at following interrupt routines for capture/compare and uart receivevoid TIM1_CC_IRQHandler(void){ uint32_t break_time, mab_time; TIM_ClearITPendingBit(TIM1, TIM_IT_CC1); break_time = TIM_GetCapture...

USB Library 2.1.0 USBH_USR_DeviceDisconnected Problem ?

Posted on March 20, 2013 at 00:32Hi. I use stm32f105 and STM32_F105-07_F2xx_USB-Host-Device_Lib_V2.0.0 usb library and i can handle  USBH_USR_DeviceDisconnected event when USBH_Process detects any Flash Disk when application starts.But when i try to...

irmakci by Associate II
  • 1912 Views
  • 2 replies
  • 0 kudos